ls1028ard secure boot failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1028ard secure boot failed

3,732 Views
540915622
Contributor III

The lsdk version is :flexbuild_lsdk2004_update_290520

I use this  command "flex-builder -i mkfw -m ls1028ardb -b xspi -s" and "flex-builder -i mkfw -m ls1028ardb -b sd -s" to generate SD card and xspi boot image .

Then use "flex-installer -f /mnt/firmware_ls1028ardb_uboot_xspiboot_secure.img -d /dev/mtdblock0" and "flex-installer -f /mnt/firmware_ls1028ardb_uboot_sdboot_secure.img -d /dev/mmcblk0" to deploy.

When I set to the corresponding startup mode, I can’t start, and there is no output from the serial port. 

Labels (2)
0 Kudos
Reply
6 Replies

3,643 Views
yipingwang
NXP TechSupport
NXP TechSupport

CodeWarrior TAP with CCS is used in the prototype design stage. In the production stage, you could write OTPMK and SRK keys to shadow registers under u-boot and blow them to fuse arrays permanently.

0 Kudos
Reply

3,643 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to section "6.1.5 Procedure to run secure boot" in document "Layerscape Software Development Kit User Guide 20.04" downloaded from" Layerscape SDK | NXP 

0 Kudos
Reply

3,644 Views
540915622
Contributor III

You can send me a SD card secure boot image ?

0 Kudos
Reply

3,644 Views
540915622
Contributor III

I refer to this document, there is no safe boot procedure for ls1028 in the document.

pastedImage_1.png

0 Kudos
Reply

3,643 Views
yipingwang
NXP TechSupport
NXP TechSupport

To below OTPMK, put jumper on J28 (TA_PROG_SFP) to supply 1.8 V to PROG_SFP

0 Kudos
Reply

3,643 Views
540915622
Contributor III

The following operations must be configured using codewarror and CW TAP?

Is there no other configuration method? Is it too troublesome to operate in a production environment?

0 Kudos
Reply