Hi,
We have a ls1028 customer board, build the system with OpenIL V1.10 ,used the configs nxp_ls1028ardb-64b_defconfig. When reboot the system, the print log is normal, but the system is stuck at the end of the exiting.
[root@LS1028ARDB ~] # reboot
Stopping Netopeer2-server: OK
- SSH hostkey found, no need to generate a new one.
Stopping rootfs-resize: OK
Stopping sysrepo-tsn: OK
Stopping sysrepo-plugind: OK
Stopping sysrepod: OK
Stopping sshd: OK
Stopping dhcpcd...
stopped /sbin/dhcpcd (pid 361)
Stopping network: OK
Stopping system message bus: done
Stopping haveged: stopped /usr/sbin/haveged (pid 294)
OK
Saving random seed: OK
Stopping klogd: OK
Stopping syslogd: OK
umount: devtmpfs busy - remounted read-only
[ 20.905084] 001: EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
The system is going down NOW!
Sent SIGTERM to all processes
logout
Sent SIGKILL to all processes
Requesting system reboot
[ 22.912562] 000: kvm: exiting hardware virtualization