ls1028 can't reboot

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1028 can't reboot

613 Views
Gnimis
Contributor II

Hi,

We have a ls1028 customer  board, build the system with OpenIL V1.10 ,used the configs nxp_ls1028ardb-64b_defconfig. When reboot the system, the print log is normal, but the system is stuck at the end of the exiting.

[root@LS1028ARDB ~] # reboot

Stopping Netopeer2-server: OK
- SSH hostkey found, no need to generate a new one.
Stopping rootfs-resize: OK
Stopping sysrepo-tsn: OK
Stopping sysrepo-plugind: OK
Stopping sysrepod: OK
Stopping sshd: OK
Stopping dhcpcd...
stopped /sbin/dhcpcd (pid 361)
Stopping network: OK
Stopping system message bus: done
Stopping haveged: stopped /usr/sbin/haveged (pid 294)
OK
Saving random seed: OK
Stopping klogd: OK
Stopping syslogd: OK
umount: devtmpfs busy - remounted read-only
[ 20.905084] 001: EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
The system is going down NOW!
Sent SIGTERM to all processes
logout
Sent SIGKILL to all processes
Requesting system reboot
[ 22.912562] 000: kvm: exiting hardware virtualization

Tags (3)
0 Kudos
1 Reply

595 Views
yipingwang
NXP TechSupport
NXP TechSupport

I confirmed with the testing team, they didn't encounter reboot problem on ls1028ardb in OpenIL V1.10 testing.

Please check whether this problem is caused by your hardware, please check whether "reset" command can be executed successfully under u-boot.

0 Kudos