ls1021a iot "bitbake linux-ls1 -c menuconfig" using openSUSE-project-13.2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ls1021a iot "bitbake linux-ls1 -c menuconfig" using openSUSE-project-13.2

810 Views
williamanderson
Contributor III

I am using openSUSE-project-13.2 as my build platform for the LS1021A IOT board.  I have built the fsl-image-full target without problems but I now want to change the kernel config. The above command does not pop open a shell window and reports no errors.  Sometimes I see a very quick flash of a window for an instant.  The output is included below.  I assume there must be a unresolved package dependency or other environment issue.

Any suggestions

Thanks

Bill

> bitbake linux-ls1 -c menuconfig
WARNING: Host distribution "openSUSE-project-13.2" has not been validated with this version of the build system; you may possibly experience unexpected failures. It is recommended that you use a tested distribution.
Loading cache: 100% |#############################################################################################################################################| ETA: 00:00:00
Loaded 2223 entries from dependency cache.
WARNING: No recipes available for:
/opt/nxpdev/QorIQ-SDK-V1.7/Freescale-Linux-SDK-for-LS1021A-IOT-Rev2-v0.4-20150907-yocto.iso/meta-rds/recipes-kernel/linux/linux-qoriq_3.12.bbappend
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.22.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "openSUSE-project-13.2"
TARGET_SYS = "arm-fsl-linux-gnueabi"
MACHINE = "ls1021aiot"
DISTRO = "fsl-networking"
DISTRO_VERSION = "QorIQ-SDK-V1.8"
TUNE_FEATURES = "armv7a vfp neon callconvention-hard cortexa7"
TARGET_FPU = "vfp-neon"
meta
meta-yocto
meta-yocto-bsp = "daisy:be8db4011cae47467e708c767d6ac02795bad02d"
meta-rds = "master:9849ad5c126ac49631a2586ad28ba0d623920b32"
meta-fsl-arm = "daisy:b62a7bb8c1c957e5b9112637f918cf645051b29a"
meta-fsl-networking = "daisy:33a46506e3505bdea7c57a8b2ed69330afc9b927"
meta-fsl-toolchain = "daisy:a253b3594d8d9e0a4ed869d1fb502c395c4438ac"
meta-virtualization = "daisy:df44ec7a68c8e4b713a458a5b93e903103dea85c"
meta-oe
meta-networking
meta-perl
toolchain-layer = "daisy:4a44c4107899363b22c01eb5621b0c86db1c659c"
meta-java = "daisy:65c89b93fa9d4c89e1dfb5b795075cbadb541009"
meta-linaro-toolchain = "daisy:9e742fbb8cbb6d2087fb41429a77fcf0ce50dbb8"
meta-security = "daisy:9f4c3849521465b459845dcc1a7a885bacaae9d9"

NOTE: Preparing runqueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
NOTE: Tasks Summary: Attempted 220 tasks of which 219 didn't need to be rerun and all succeeded.

Summary: There were 2 WARNING messages shown.
wanderson@curly:/opt/nxpdev/QorIQ-SDK-V1.7/Freescale-Linux-SDK-for-LS1021A-IOT-Rev2-v0.4-20150907-yocto.iso/build_ls1021aiot_release>

Labels (1)
0 Kudos
Reply
0 Replies