我们使用LS1012的USB3.0挂载一个5G模组,然后网络经1012的以太网接外部服务器,期间路由转发直接用IPTABL设置规则,目前发现当数据下载速率到250Mbps时候,数据转发速率上不去(5G单模组实测时候速率可以达到700Mbps),cpu空闲为0,检查过USB3.0和以太网口不是瓶颈,很可能是由于网络转发造成的,有没有方案可以对这个进行优化,
Which NXP software is in question?
Are you using ASK?
I used on ls1012a platform,and there is no use ask,In case of no use ask is there any other solutions?
Operation at near line rate speed is possible using PFE which is supported by the ASK.
In case of not using ASK directly, can I achieve the same effect if I use DPDK?
ASK is a must to use PFE.
thanks,Dpdk and ask can be used for USB or PCIe virtual Ethernet Adapter forwarding?If possible, which is is better?USB 3.0 or PCIE?