is there have a lx2160a jffs rootfs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

is there have a lx2160a jffs rootfs

731 Views
muaxi8
Contributor V

I used 512MB XSPI Flash.The root file system I'm using now is"rootfs_lsdk2012_yocto_tiny_arm64.cpio.gz", which is a  ramdisk rfs, and files created will not be saved after reboot.I was wondering if you have a JFFS rfs?

0 Kudos
3 Replies

724 Views
yipingwang
NXP TechSupport
NXP TechSupport

BR2_TARGET_ROOTFS_JFFS2=y  is defined in configs/buildroot/arm64_devel_defconfig
You could generate jffs2 rootfs filesystem with the following command.​
$ flex-builder -i mkrfs  -r buildroot:tiny
0 Kudos

708 Views
muaxi8
Contributor V

I can't download RFS, can you send me one ?

err message:

flex-builder -i mkrfs -r buildroot:tiny
INSTRUCTION: mkrfs
DISTRO TYPE: buildroot
DISTRO SCALE: tiny
Cloning into '/home/chunxi/work/0734/flexbuild_lsdk2012/packages/rfs/buildroot'...
fatal: unable to access 'https://github.com/buildroot/buildroot.git/': Failed to connect to 52.74.223.119 port 1080: Connection timed out

0 Kudos

701 Views
yipingwang
NXP TechSupport
NXP TechSupport
0 Kudos