is mSata supported on LS1021A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

is mSata supported on LS1021A

808 Views
shawnreuland
Contributor I

Hello, the LS1021A-IOT fact sheet:

http://cache.nxp.com/files/32bit/doc/fact_sheet/LS1IoTGTWYFS.pdf?fpsp=1&WT_TYPE=Fact%20Sheets&WT_VEN...

states an mSata 3.0 slot, but there is none visible on the reference board pictures. Is mSata provided by LS1021A MCU? Is it possible then to have layout with (2) PCI-E slots and (1) mSata slot?

Labels (1)
0 Kudos
1 Reply

696 Views
lunminliang
NXP Employee
NXP Employee

Hello shawn reuland,

Yes,  I think you can see it there in the picture:

pastedImage_0.png

Yes, LS1021A support Sata 3.0. It's possible to have two PCIe and one mSata.


Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos