is m-sata available on LS1020A?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

is m-sata available on LS1020A?

1,061 Views
shawnreuland
Contributor I

Hello, how is m-sata enabled with LS1020A? I see the tower dev board, TWR-LS1021A, fact sheet

http://cache.nxp.com/files/32bit/doc/fact_sheet/TWRLS1021AFS.pdf?fpsp=1&WT_TYPE=Fact%20Sheets&WT_VEN...

mentions (1) m-sata slot, and the LS1021A iot reference mentions the same m-sata slot:

http://cache.nxp.com/files/32bit/doc/fact_sheet/LS1IoTGTWYFS.pdf?fpsp=1&WT_TYPE=Fact%20Sheets&WT_VEN...

however, in both cases, it doesn't look like there is a slot on the board pics, just two plain pci-e, correct? Just want to confirm, can a design incorporate a third pci-e slot be connected to LS1020A in conjunction with its sata controller in order to support m-sata card plugins?

Labels (1)
0 Kudos
Reply
1 Reply

957 Views
ufedor
NXP Employee
NXP Employee

You wrote:

> it doesn't look like there is a slot on the board pics, just two plain pci-e, correct?

No.

Each board has dedicated SATA connector.

0 Kudos
Reply