how to poweroff on ls1028ardb

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to poweroff on ls1028ardb

602 Views
Eddy1
Contributor IV

Hi:

 When I entered the “poweroff” command, I found that it would restart in about one minute on the ls1028 platform.

$:poweroff

.......

Saving random seed: OK
Stopping klogd: OK
Stopping syslogd: OK
umount: devtmpfs busy - remounted read-only
[ 30.541566] 001: EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
The system is going down NOW!
Sent SIGTERM to all processes
logout
Sent SIGKILL to all processes
Requesting system poweroff
[ 32.550589] 000: kvm: exiting hardware virtualization
NOTICE: Fixed DDR on board

NOTICE: 4 GB DDR4, 32-bit, CL=11, ECC on
NOTICE: BL2: v1.5(release):b0d8f9e
NOTICE: BL2: Built : 09:57:04, Jun 8 2021
NOTICE: BL31: v1.5(release):b0d8f9e
NOTICE: BL31: Built : 09:57:04, Jun 8 2021
NOTICE: Welcome to LS1028 BL31 Phase

0 Kudos
3 Replies

594 Views
Pavel
NXP Employee
NXP Employee

The LS1028ARDB board does not support power off possibility from software. See the Section 2.2 in the LS1028ARDB board Reference Manual:

https://www.nxp.com/webapp/Download?colCode=LS1028ARDBRM

 

Only power switch for the LTC2955-2 provides power off for this board.

0 Kudos

589 Views
Eddy1
Contributor IV

Hi:

Will you implement software poweroff in the future?We have designed the development board according to ls1028ardb board. If we want to realize the software poweroff, do you have any suggestions?

0 Kudos

575 Views
Pavel
NXP Employee
NXP Employee

Add the R431 and the R432 on the LS1029ARDB board to generate KILL from 12V directly.

0 Kudos