how to connect tja1101 to ls1028

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

how to connect tja1101 to ls1028

Jump to solution
530 Views
jason-1117
Contributor I

Hi everyone,

 

I am new for LS1028 and I want to use it for Automotive Ethernet develop, so I need to connect 4-5 pics tja1101 to ls1028. However, tja1101 use mii/rmii and ls1028 use sgmii, how to make two chips work together(as figure show in https://community.nxp.com/t5/NXP-Designs-Knowledge-Base/Boards-and-Standard-Form-Factor/ta-p/1164256 )?

 

Thank you very much,

Best,

Jason Xu

0 Kudos
1 Solution
513 Views
Bulat
NXP Employee
NXP Employee

Unfortunately the block diagram you referred to is incorrect, the TJA1101 can not be directly connected to the LS1028. Actually the LS1028 is mostly considered for industial applications rather than for automotive ones.

Regards,

Bulat

 

 

View solution in original post

0 Kudos
1 Reply
514 Views
Bulat
NXP Employee
NXP Employee

Unfortunately the block diagram you referred to is incorrect, the TJA1101 can not be directly connected to the LS1028. Actually the LS1028 is mostly considered for industial applications rather than for automotive ones.

Regards,

Bulat

 

 

0 Kudos