ext4load from usb is failing.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ext4load from usb is failing.

240 Views
sbijjal
Contributor I

rcpZ=> usb start
starting USB...
---- init USB low level ----

USB1:
Register 200017f NbrPorts 2
Starting the controller
USB XHCI 1.00
USB1 successfully started.

USB2:
this is not a DesignWare USB3 DRD Core
Failed to initialize xhci
probe failed, error -1

USB3:
this is not a DesignWare USB3 DRD Core
Failed to initialize xhci
probe failed, error -1

---- scan USB buses (search HUBs) ----
USB1:
scanning bus 0 for devices... 2 USB Device(s) found

scanning usb for storage devices... 1 Storage Device(s) found

rcpZ=> ext4ls usb 0:1 1/
<DIR> 1024 .
<DIR> 1024 ..
0 9865846 fitImage-rcpZ

rcpZ=> ext4load usb 0:1 0xa0000000 /1/fitImage-rcpIa
usb_control_msg: error: submit_control_msg() returns err=-110
usb_control_msg: error: submit_control_msg() returns err=-110
WARN halted endpoint, queueing URB anyway.
Unexpected XHCI event TRB, skipping... (fbc4cff0 00000000 13000000 01008400)
BUG at drivers/usb/host/xhci-ring.c:495/abort_td()!
BUG!
resetting ...

0 Kudos
Reply
1 Reply

209 Views
June_Lu
NXP TechSupport
NXP TechSupport

Would you kindly share the MPU part number and SW version, thanks

0 Kudos
Reply