early debug prints in uboot for ls1088ardb

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

early debug prints in uboot for ls1088ardb

1,587件の閲覧回数
anandkrs
Contributor I

How to enable the early prints in uboot for debugging, What is base address for the uart to use. Is there any sample / patch available to do the early stage debugging using the console prints. I am using u-boot 2018.09 version.

ラベル(2)
0 件の賞賛
返信
1 返信

1,321件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Hello Anand Singh,

If you have CodeWarrior TAP, you could download and install CodeWarrior for ARMv8(CW4NET_v2019.01) to debug u-boot from the beginning, please refer to the section "2. Debug u-boot with CodeWarrior for ARMv8" in Use CodeWarrior for ARMv8 to Debug U-boot and Linux Kernel and Bring up Bare Boards.

Thanks,

Yiping

 

 

0 件の賞賛
返信