eSDHC of LS1021a eMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eSDHC of LS1021a eMMC

734 Views
jiye
Contributor V

Hi,

if my only boot source of  ls1021a stand alone chip is eMMC do I need to specify the boot mode in the RCW source file again?

pastedImage_1.png

Also from the ls1021ARM reference manual

Section 4.4.1

The device samples the RCW source POR configuration inputs (cfg_rcw_src[0:n])
on deassertion of PORESET_B to determine the RCW source. Note that the POR
configuration inputs are sampled only on a PORESET_B.

How can I sample POR configuration inputs on my standalone application is this done automatically after deassertion of PORESET_B?

Labels (1)
0 Kudos
1 Reply

623 Views
Pavel
NXP Employee
NXP Employee

The cfg_rcw_src signals are used for RCW source.

 

The LS1021a SDHC is RCW source fir 0_0100_0000 setting of the cfg_rcw_src. See the Table 4-9 of the LS1021a Reference Manual.

 

The LS1021a RCW provides configuration for SDHC pin assigning of the LS1021a.

See the SDHC_BASE and SDHC_EXT fields in the LS1021a RCW.

The PBI_SRC RCW bits are used for setting SD/MMC as PBL initialization source.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos