code warrior tap error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

code warrior tap error

7,288 次查看
rashmikj
Contributor III

Hi,

When i try to connect code warrior tap to LS1046ardb , I am getting the following error.

Kindly help

标记 (1)
0 项奖励
回复
6 回复数

7,279 次查看
ufedor
NXP Employee
NXP Employee

Which Target Configuration is selected?

Run Diagnose Connection:

Diagnose.jpg

0 项奖励
回复

7,269 次查看
rashmikj
Contributor III

Please find attached error also when i scan for probe its unable to scan the codewarrior tap usb connected.

0 项奖励
回复

7,265 次查看
ufedor
NXP Employee
NXP Employee

Press "Connection Diagnostics" button and provide the Connection Diagnostics tab screenshot.

0 项奖励
回复

7,257 次查看
rashmikj
Contributor III

Please find attached screenshot.

0 项奖励
回复

7,251 次查看
ufedor
NXP Employee
NXP Employee

Please try the following steps:

1) completely uninstall CodeWarrior IDE

2) disable anti-virus application(s)

3) install latest Java

4) install CodeWarrior IDE

5) enable anti-virus application(s)

 

In case of further questions capture complete Help message as text.

0 项奖励
回复

7,242 次查看
rashmikj
Contributor III

After disabling the anti virus and reinstalling the code warrior , it is working fine.

Thank you.

标记 (1)
0 项奖励
回复