Yocto build: I have build a image for ls1043ardb, how to boot from build image ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Yocto build: I have build a image for ls1043ardb, how to boot from build image ?

1,120件の閲覧回数
iyyanar
Contributor I

Yocto build: I have build a image for ls1043ardb, how to boot from build image ?

ラベル(2)
0 件の賞賛
返信
1 返信

955件の閲覧回数
Pavel
NXP Employee
NXP Employee

See the Sections 4.4.7.8 and 4.4.7.9 of SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 

Use also SD card for booting.

Write u-boot binary file and fman microcode to SD card on your Linux PC and use this SD card for booting.

Write this u-boot to SD card using Linux on host PC.

Use the following command on this Linux host PC:

sudo dd if=uboot_ls1043ardb_sdcard.bin of=/dev/sdc1 bs=512 seek=8  

 

sudo dd if=fman_ucode_ls1043a_4_18.bin of=/dev/sdd seek=0x820 bs=512

 

Set the following SW setting on your LS1043ARDB board:

SW4[1-8] +SW5[1] = 0b'00100000_0  SW3[8]=0.

 

Connect your LS1043ARDB board to host PC. Use terminal software as console.

Insert this SD card and switch power on.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信