XFI SERDES channels for 1GbE/10GbE SFP+ operation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

XFI SERDES channels for 1GbE/10GbE SFP+ operation

ソリューションへジャンプ
1,667件の閲覧回数
luukmeijles
Contributor I

Hi,

I am investigating the ability to connect the XFI interface of the LS1046A with a retimer to a SFP+ cage.  The SFP+ module will be 1G/10G dual mode and I was wondering if the XFI interface could directly interface with the 1G signal or if it should be converted to 10G.

Thank you,

Luuk

タグ(1)
0 件の賞賛
返信
1 解決策
1,661件の閲覧回数
ufedor
NXP Employee
NXP Employee

XFI is a single-speed 10G interface - it cannot support 1G target.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,662件の閲覧回数
ufedor
NXP Employee
NXP Employee

XFI is a single-speed 10G interface - it cannot support 1G target.

0 件の賞賛
返信