XFI SERDES channels for 1GbE/10GbE SFP+ operation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

XFI SERDES channels for 1GbE/10GbE SFP+ operation

Jump to solution
2,275 Views
luukmeijles
Contributor I

Hi,

I am investigating the ability to connect the XFI interface of the LS1046A with a retimer to a SFP+ cage.  The SFP+ module will be 1G/10G dual mode and I was wondering if the XFI interface could directly interface with the 1G signal or if it should be converted to 10G.

Thank you,

Luuk

Tags (1)
0 Kudos
Reply
1 Solution
2,269 Views
ufedor
NXP Employee
NXP Employee

XFI is a single-speed 10G interface - it cannot support 1G target.

View solution in original post

0 Kudos
Reply
1 Reply
2,270 Views
ufedor
NXP Employee
NXP Employee

XFI is a single-speed 10G interface - it cannot support 1G target.

0 Kudos
Reply