Which pin is mapped to GPIO in TWR-LS1021A?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which pin is mapped to GPIO in TWR-LS1021A?

Jump to solution
2,090 Views
takumishimada
Contributor II

I would like to use GPIO on TWR-LS1021A.

I read TWR-LS1021A Reference Manual 2.21 and 3.1, and understood some pin of card edge connector is mapped to GPIO.

But I cannot understand what "GPIOn" (e.g. GPIO14) in the Table 3-1 means.

In TWR-LS1021A, there are 4 GPIO module and each of them has its own port.

Therefore, it seems it should be written as "GPIO_m[n]".

In the table of the reference manual, which port is mapped to "GPIOn"?

Regards,

Takumi

Labels (1)
Tags (2)
0 Kudos
1 Solution
1,404 Views
Pavel
NXP Employee
NXP Employee

The LS1021A RCW provides pin assignment between main function and alternate functions. Use the LS1021A RCW for pins assignment as alternate function (GPIO).


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
5 Replies
1,404 Views
Pavel
NXP Employee
NXP Employee

The TWR-LS1021A uses I2C I/O port as GPIO expander. Find the U26 (PCA9555BS) on the TWR-LS-1021A board.

The GPIO14 is GPIO from this I2C I/O port.

Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,404 Views
takumishimada
Contributor II

Thanks Pavel.

I want to know where other ports are mapped.

Where are GPIO1 ~ GPIO31 mapped?

And which document can we refer to know where these ports are mapped?

Regards,

Takumi

0 Kudos
1,404 Views
Pavel
NXP Employee
NXP Employee

Most of GPIO signals are available from CPLD on the TWR-LS1021A board.

There is a few GPIO from the LS1021. Find the FTM1_QD_PHA_GPIO3_13 or FTM1_QD_PHB_GPIO3_14 signals on the TWR-LS1021A board.


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,404 Views
takumishimada
Contributor II

I found the signal description chapter in LS1021A Reference Manual.

But this chapter doesn't describe which pin the signal is sent to.

I want to send some signal to other devices.

Regards,

Takumi

0 Kudos
1,405 Views
Pavel
NXP Employee
NXP Employee

The LS1021A RCW provides pin assignment between main function and alternate functions. Use the LS1021A RCW for pins assignment as alternate function (GPIO).


Have a great day,
Pavel

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos