Which SDK should use for FRWY-LS1046A-PA?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Which SDK should use for FRWY-LS1046A-PA?

1,654 Views
pomepome11
Contributor III

In the page below, two SDKs are listed.
https://www.nxp.com/design/qoriq-developer-resources/ls1046a-freeway-board:FRWY-LS1046A
- Layerscape Software Development Kit - v19.06
- Layerscape SDK for FRWY-LS1046A

The former is marked as "RDB only" in the page, but the user guide says FRWY-LS1046A is supported on page 44.

So, my question is:

Which SDK is recommended to use?

And, what is the difference of these SDKs in case building images for FRWY-LS1046A ?

Labels (1)
Tags (1)
0 Kudos
Reply
2 Replies

1,508 Views
ufedor
NXP Employee
NXP Employee

Currently FRWY-LS1046A is supported only by the LSDK v19.06.

0 Kudos
Reply

1,508 Views
pomepome11
Contributor III

OK, i should use "Layerscape Software Development Kit - v19.06.", right ?

If so, what is "Layerscape SDK for FRWY-LS1046A" ?

0 Kudos
Reply