Where should I post bugs that I've discovered in the Layerscape SDK?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where should I post bugs that I've discovered in the Layerscape SDK?

Jump to solution
780 Views
kuta42
Contributor III

I've discovered several bugs in the Layerscape SDK v17.12 . Is there a bug tracking system to which I can post them? If not, then how should they be reported?

Labels (1)
0 Kudos
Reply
1 Solution
656 Views
Pavel
NXP Employee
NXP Employee

The simplest way if technical request will be created about these bugs. See the following page:

https://community.nxp.com/thread/381898


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
657 Views
Pavel
NXP Employee
NXP Employee

The simplest way if technical request will be created about these bugs. See the following page:

https://community.nxp.com/thread/381898


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------