Where is the driver named "sec-v4.0-mon"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where is the driver named "sec-v4.0-mon"

Jump to solution
2,807 Views
jasonhendrix
Contributor V

I'm trying to enable the ls1021a on-chip RTC in Linux.  According to the binding text, the sec_mon unit should be bound to the sec-v4.0-mon driver.  But I cannot find where that driver is implemented.  sec-v4.0-mon-rtc-lp is implemented in snvs_rtc.c as expected.  Where can I get the driver named "sec-v4.0-mon" (or and equivalent) for accessing the ls1021a Security Monitor?  Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
1,433 Views
jasonhendrix
Contributor V

Yes, simple-bus is valid, and works as the fall-back for the non-existent "sec-v4.0-mon" driver.  See my other post in the NXP community for more details on the device tree.

View solution in original post

0 Kudos
Reply
3 Replies
1,433 Views
jasonhendrix
Contributor V

I found this thread, which seems to state that there is no sec-v4.0-mon driver.  The fallback compatible "simple-bus" is supposed to allow access to the rtc_lp device. 

[PATCH v2] rtc: snvs: add Freescale rtc-snvs driver

Does anyone know if "simple-bus" is a valid fallback compatible; I've seen people recommend "syscon" as well.  Thanks.

0 Kudos
Reply
1,434 Views
jasonhendrix
Contributor V

Yes, simple-bus is valid, and works as the fall-back for the non-existent "sec-v4.0-mon" driver.  See my other post in the NXP community for more details on the device tree.

0 Kudos
Reply
1,433 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Jason Hendrix,

SNVS RTC is not formally supported in LS1021x Linux SDK, you could refer to the dts for imx6 arch/arm/boot/dts/imx6sl.dtsi.

For hardware design, please refer to  LS1021AQDS.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply