Where can I find the original RCW and U-Boot image that came with TWR-LS1021A (rev D)?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Where can I find the original RCW and U-Boot image that came with TWR-LS1021A (rev D)?

1,397 Views
dandolf
Contributor II

The RCW and U-Boot image has been replaced on both banks of the TWR-LS1021A, Rev D.  However, I would like to use the original RCW and U-Boot image that the board came with.  Can I have a copy of those so I can write it to the board?  Thanks!

Labels (1)
0 Kudos
Reply
2 Replies

1,091 Views
alexander_yakov
NXP Employee
NXP Employee

Board flash binary and rcw may be found in Linux SDK, "image" iso. For LS1021A processor please look "CORTEXA7":

"QorIQ Linux SDK v2.0 CORTEXA7 IMAGE.iso"

Linux® SDK for QorIQ ® Processors|NXP 


Have a great day,
Alexander
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

1,091 Views
swanandpurankar
Contributor III

It is present in the Pen Drive which you must have received along with the board. Or Even in the SD card. You can find "u-boot.bin" file. That contains default RCW