What are the best debugger options for LS1046A Reference Board? What kind of emulators/probes are needed for JTAG Support?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What are the best debugger options for LS1046A Reference Board? What kind of emulators/probes are needed for JTAG Support?

Jump to solution
3,134 Views
shamanth_kudali
Contributor II

Wanted to know if the JTAG port on the board is the best debugging option and how to interface with this JTAG port?

Labels (2)
1 Solution
2,717 Views
Pavel
NXP Employee
NXP Employee

The LS1046A JTAG/COP interface usually is used for debugging.

 

NXP offers CodeWarrior Networking Application for development code and debugging on the LS1046A boards:

https://www.nxp.com/products/processors-and-microcontrollers/additional-processors-and-mcus/digital-...

 

This CodeWarrior uses CodeWarrior TAP for code loading and debugging:

https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-t...

 

and QorIQ LS Processor Probe Tips for CodeWarrior TAP:

https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-t...

 

CodeWarrior TAP uses JTAG/COP connection to the LS1046a.

 

See also TRACE32 from Lauterbach:

https://www.lauterbach.com/frames.html?home.html

 

and debuggers on the following page:

https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/qoriq-lay...

 
Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
2 Replies
2,717 Views
shamanth_kudali
Contributor II

Thanks for the response Pavel. 

Had a few more questions. 

Query 1: Will the combination of Code Warrior, TAP and QorIQ LS Processor Probe Tips be sufficient for the below debugging features?

  1. Tracing and obtaining a trace log of execution.
  2. Single Step Debugging
  3. Breakpoints – How many?

 

Query 2: Is there any other open source IDE available as an alternative for Code Warrior?

If no, what are the licensing options for Code Warrior?

2,718 Views
Pavel
NXP Employee
NXP Employee

The LS1046A JTAG/COP interface usually is used for debugging.

 

NXP offers CodeWarrior Networking Application for development code and debugging on the LS1046A boards:

https://www.nxp.com/products/processors-and-microcontrollers/additional-processors-and-mcus/digital-...

 

This CodeWarrior uses CodeWarrior TAP for code loading and debugging:

https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-t...

 

and QorIQ LS Processor Probe Tips for CodeWarrior TAP:

https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-t...

 

CodeWarrior TAP uses JTAG/COP connection to the LS1046a.

 

See also TRACE32 from Lauterbach:

https://www.lauterbach.com/frames.html?home.html

 

and debuggers on the following page:

https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/qoriq-lay...

 
Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply