What are the best debugger options for LS1046A Reference Board? What kind of emulators/probes are needed for JTAG Support?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What are the best debugger options for LS1046A Reference Board? What kind of emulators/probes are needed for JTAG Support?

ソリューションへジャンプ
3,131件の閲覧回数
shamanth_kudali
Contributor II

Wanted to know if the JTAG port on the board is the best debugging option and how to interface with this JTAG port?

ラベル(2)
1 解決策
2,714件の閲覧回数
Pavel
NXP Employee
NXP Employee

The LS1046A JTAG/COP interface usually is used for debugging.

 

NXP offers CodeWarrior Networking Application for development code and debugging on the LS1046A boards:

https://www.nxp.com/products/processors-and-microcontrollers/additional-processors-and-mcus/digital-...

 

This CodeWarrior uses CodeWarrior TAP for code loading and debugging:

https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-t...

 

and QorIQ LS Processor Probe Tips for CodeWarrior TAP:

https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-t...

 

CodeWarrior TAP uses JTAG/COP connection to the LS1046a.

 

See also TRACE32 from Lauterbach:

https://www.lauterbach.com/frames.html?home.html

 

and debuggers on the following page:

https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/qoriq-lay...

 
Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,714件の閲覧回数
shamanth_kudali
Contributor II

Thanks for the response Pavel. 

Had a few more questions. 

Query 1: Will the combination of Code Warrior, TAP and QorIQ LS Processor Probe Tips be sufficient for the below debugging features?

  1. Tracing and obtaining a trace log of execution.
  2. Single Step Debugging
  3. Breakpoints – How many?

 

Query 2: Is there any other open source IDE available as an alternative for Code Warrior?

If no, what are the licensing options for Code Warrior?

2,715件の閲覧回数
Pavel
NXP Employee
NXP Employee

The LS1046A JTAG/COP interface usually is used for debugging.

 

NXP offers CodeWarrior Networking Application for development code and debugging on the LS1046A boards:

https://www.nxp.com/products/processors-and-microcontrollers/additional-processors-and-mcus/digital-...

 

This CodeWarrior uses CodeWarrior TAP for code loading and debugging:

https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-t...

 

and QorIQ LS Processor Probe Tips for CodeWarrior TAP:

https://www.nxp.com/support/developer-resources/software-development-tools/codewarrior-development-t...

 

CodeWarrior TAP uses JTAG/COP connection to the LS1046a.

 

See also TRACE32 from Lauterbach:

https://www.lauterbach.com/frames.html?home.html

 

and debuggers on the following page:

https://www.nxp.com/products/processors-and-microcontrollers/arm-based-processors-and-mcus/qoriq-lay...

 
Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信