WARNING: Failed to fetch URL ...

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

WARNING: Failed to fetch URL ...

跳至解决方案
11,692 次查看
scottywimberley
Contributor I

WARNING: Failed to fetch URL ...

The following begins with the command and shows the failures:

~/QorIQ-SDK-V2.0-20160527-yocto/build_ls1021atwr$ bitbake -c cleansstate u-boot
Loading cache: 100% |#########################################################| ETA:  00:00:00
Loaded 3425 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION        = "1.28.0"
BUILD_SYS         = "x86_64-linux"
NATIVELSBSTRING   = "Ubuntu-14.04"
TARGET_SYS        = "arm-fsl-linux-gnueabi"
MACHINE           = "ls1021atwr"
DISTRO            = "fsl-qoriq"
DISTRO_VERSION    = "2.0"
TUNE_FEATURES     = "arm armv7a vfp neon callconvention-hard cortexa7"
TARGET_FPU        = "vfp-neon"
meta             
meta-yocto       
meta-yocto-bsp    = "HEAD:9a211a4a2c1bfcb292dc97d8dcac149bca9e3f1b"
meta-oe          
meta-multimedia  
meta-gnome       
meta-networking  
meta-perl        
meta-python      
meta-ruby        
meta-filesystems 
meta-webserver   
meta-xfce         = "HEAD:dc5634968b270dde250690609f0015f881db81f2"
meta-freescale    = "HEAD:7facbdb726e2dda0515e084c2066a4b8dd99c6d2"
meta-freescale-internal = "HEAD:4829293f807e35a1111e79763294fc8b98b97810"
meta-freescale-extra = "HEAD:bee911b027e0480b034674d0ddee3fcb06d2e985"
meta-virtualization = "HEAD:042425c1d98bdd7e44a62789bd03b375045266f5"
meta-java         = "HEAD:8b776ac68f9af4596be3824152bcf0bc6b67fa1d"
meta-openstack   
meta-openstack-aio-deploy
meta-openstack-compute-deploy
meta-openstack-compute-test-config
meta-openstack-controller-deploy
meta-openstack-controller-test-config
meta-openstack-qemu
meta-openstack-swift-deploy
meta-cloud-services = "HEAD:d8bc0d92d0f741e2ea1e6d3d9bc6b7a091d03cfb"
meta-security     = "HEAD:f9367e71f923fc7d2fb600208e2b97535ea41777"
meta-linaro-toolchain = "HEAD:10b71bed9cfe76baa22c72806ff814cf85c2f73b"

NOTE: Preparing RunQueue
NOTE: Executing RunQueue Tasks
NOTE: Tasks Summary: Attempted 2 tasks of which 0 didn't need to be rerun and all succeeded.

~/QorIQ-SDK-V2.0-20160527-yocto/build_ls1021atwr$ bitbake -c patch u-boot
Loading cache: 100% |#########################################################| ETA:  00:00:00
Loaded 3425 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION        = "1.28.0"
BUILD_SYS         = "x86_64-linux"
NATIVELSBSTRING   = "Ubuntu-14.04"
TARGET_SYS        = "arm-fsl-linux-gnueabi"
MACHINE           = "ls1021atwr"
DISTRO            = "fsl-qoriq"
DISTRO_VERSION    = "2.0"
TUNE_FEATURES     = "arm armv7a vfp neon callconvention-hard cortexa7"
TARGET_FPU        = "vfp-neon"
meta             
meta-yocto       
meta-yocto-bsp    = "HEAD:9a211a4a2c1bfcb292dc97d8dcac149bca9e3f1b"
meta-oe          
meta-multimedia  
meta-gnome       
meta-networking  
meta-perl        
meta-python      
meta-ruby        
meta-filesystems 
meta-webserver   
meta-xfce         = "HEAD:dc5634968b270dde250690609f0015f881db81f2"
meta-freescale    = "HEAD:7facbdb726e2dda0515e084c2066a4b8dd99c6d2"
meta-freescale-internal = "HEAD:4829293f807e35a1111e79763294fc8b98b97810"
meta-freescale-extra = "HEAD:bee911b027e0480b034674d0ddee3fcb06d2e985"
meta-virtualization = "HEAD:042425c1d98bdd7e44a62789bd03b375045266f5"
meta-java         = "HEAD:8b776ac68f9af4596be3824152bcf0bc6b67fa1d"
meta-openstack   
meta-openstack-aio-deploy
meta-openstack-compute-deploy
meta-openstack-compute-test-config
meta-openstack-controller-deploy
meta-openstack-controller-test-config
meta-openstack-qemu
meta-openstack-swift-deploy
meta-cloud-services = "HEAD:d8bc0d92d0f741e2ea1e6d3d9bc6b7a091d03cfb"
meta-security     = "HEAD:f9367e71f923fc7d2fb600208e2b97535ea41777"
meta-linaro-toolchain = "HEAD:10b71bed9cfe76baa22c72806ff814cf85c2f73b"

NOTE: Preparing RunQueue
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
WARNING: Failed to fetch URL git://git.freescale.com/ppc/sdk/u-boot.git;branch=sdk-v2.0.x, attempting MIRRORS if available
ERROR: Fetcher failure: Unable to find revision a9b437f50e2051f8d42ec9e1a6df52de4bc00e1e in branch sdk-v2.0.x even from upstream
ERROR: Function failed: Fetcher failure for URL: 'git://git.freescale.com/ppc/sdk/u-boot.git;branch=sdk-v2.0.x'. Unable to fetch URL from any source.
ERROR: Logfile of failure stored in: /home/scott/QorIQ-SDK-V2.0-20160527-yocto/build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux-gnueabi/u-boot-qoriq/2016.01+fslgit-r0/temp/log.do_fetch.5296
ERROR: Task 2 (/home/scott/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-bsp/u-boot/u-boot-qoriq_2016.01.bb, do_fetch) failed with exit code '1'
NOTE: Tasks Summary: Attempted 8 tasks of which 7 didn't need to be rerun and 1 failed.
No currently running tasks (7 of 10)

Summary: 1 task failed:
  /home/scott/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-bsp/u-boot/u-boot-qoriq_2016.01.bb, do_fetch
Summary: There was 1 WARNING message shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

标签 (1)
0 项奖励
回复
1 解答
8,167 次查看
Pavel
NXP Employee
NXP Employee

Remove the build_ls1021atwr folder and issue again the command: . ./fsl-setup-env -m ls1021atwr

Start bitbake agin.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
3 回复数
8,168 次查看
Pavel
NXP Employee
NXP Employee

Remove the build_ls1021atwr folder and issue again the command: . ./fsl-setup-env -m ls1021atwr

Start bitbake agin.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
8,166 次查看
Pavel
NXP Employee
NXP Employee

Test your building using the following patch:

http://git.freescale.com/git/cgit.cgi/yocto/meta-nxp-npi.git/commit/?h=jethro-sdk-v2.0-ga-17.03

 

Attached file contains corrected linux-qoriq_4.1.bbappend file. Path for this file is the following:

/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-nxp-npi-1703/recipes-kernel/linux


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复
8,166 次查看
scottywimberley
Contributor I

Thank you Pavel,

I placed the file "linux-qoriq_4.1.bbappend" in the following location:

/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-nxp-npi-

1703/recipes-kernel/linux

Then: . ./fsl-setup-env -m ls1021atwr

Result:

WARNING: Failed to fetch URL git://

git.freescale.com/ppc/sdk/u-boot.git;branch=sdk-v2.0.x, attempting MIRRORS

if available

ERROR: Fetcher failure: Unable to find revision

a9b437f50e2051f8d42ec9e1a6df52de4bc00e1e in branch sdk-v2.0.x even from

upstream

ERROR: Function failed: Fetcher failure for URL: 'git://

git.freescale.com/ppc/sdk/u-boot.git;branch=sdk-v2.0.x'. Unable to fetch

URL from any source.

ERROR: Logfile of failure stored in:

/home/scott/QorIQ-SDK-V2.0-20160527-yocto/build_ls1021atwr/tmp/work/ls1021atwr-fsl-linux-gnueabi/u-boot-qoriq/2016.01+fslgit-r0/temp/log.do_fetch.3989

ERROR: Task 65

(/home/scott/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-bsp/u-boot/

u-boot-qoriq_2016.01.bb, do_fetch) failed with exit code '1'

0 项奖励
回复