VR500 PMIC SW1 Current Insufficient For LS1028A Applications

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

VR500 PMIC SW1 Current Insufficient For LS1028A Applications

跳至解决方案
827 次查看
jimmymm
Contributor II

I am in the process of implementing the power scheme to our custom LS1028A application. I saw from the LS1028A Reference Design Board that NXP utilizes and recommends the VR500 PMIC, specifically the MC34VR500V9ES, for the LS1028A application. In the VR500 datasheet, the SW1 output is described to supply the LS1028A's VDD core (1.0V/0.9V) with a max current of 4.5 Amps. 

According to the LS1028A Design Checklist "Table 7. Typical use case power at 65 C", every LS1028A configuration exceeds the current available from the VR500 SW1 output. I find it unusual that the PMIC recommended for this processor is not capable of providing sufficient VDD current under load. 

Is this the right PMIC for the LS1028A, or is there another PMIC available that is capable of providing sufficient power without having to use another separate switching power supply?

标签 (1)
0 项奖励
1 解答
778 次查看
ufedor
NXP Employee
NXP Employee

It is reasonable to refer to the QorIQ LS1028A Reference Design Board Reference Manual, 2.2 Power supplies where it is shown that VDD is provided by LTC7151S:

UM.jpg

and the RDB schematics:

SCH.jpg

在原帖中查看解决方案

0 项奖励
1 回复
779 次查看
ufedor
NXP Employee
NXP Employee

It is reasonable to refer to the QorIQ LS1028A Reference Design Board Reference Manual, 2.2 Power supplies where it is shown that VDD is provided by LTC7151S:

UM.jpg

and the RDB schematics:

SCH.jpg

0 项奖励