Using our board with LS1043 processor

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Using our board with LS1043 processor

1,047 次查看
carlos-m-ribeiro
Contributor I

Good morning,

If possible we would like to clarify a matter with NXP and we need your help.

In our company, we will have an real scenario that uses ls1043 processor in our boards. If we need only to use the U-BOOT for QSPI, the Frame Manager's (FMan), the Period and Pulse Accumulator (PPA) and the Reset Configuration Word (RCW), which should be the most recommended command ls1043aqds of flex-builder and which binaries should be flash into our board. Another important thing is to know which files are dedicated to our board.

 

Best regards

 

 

0 项奖励
回复
3 回复数

1,025 次查看
ufedor
NXP Employee
NXP Employee

> Period and Pulse Accumulator (PPA)

PPA means Primary Protected Application. It is not supported for the LS1043A in the latest LSDK.

Considering requested functionality it will be supported by the composite firmware image generated by flexbuilder - please read the Layerscape Linux SDK Documentation:

https://www.nxp.com/design/software/embedded-software/linux-software-and-development-tools/layerscap...

 

0 项奖励
回复

1,022 次查看
carlos-m-ribeiro
Contributor I

Thank you for your response but there was a mistake. All we need for our board is the frame manager, U-BOOT and RCW+PBI=PBL.

Best regards

0 项奖励
回复

1,039 次查看
carlos-m-ribeiro
Contributor I

NOTE: our board also need PBI-PBL.

0 项奖励
回复