USB3.0 Problem of XFRWY-LS1012A-PA

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB3.0 Problem of XFRWY-LS1012A-PA

Jump to solution
651 Views
Steve81800
Contributor II

Dear Experts,

I was trying to connect USB3.0 devices to XFRWY-LS1012A-PA, unfortunately it only has a micro USB3.0 AB connector. So I tried to connect a type-C hub (with USB-C upstream connector) with a micro USB3.0 to type-C cable. I have plugged a USB3.0 pen drive and it seems to work. However, it won't work with any USB2.0 devices. Besides, I receive the following message continuously on my console terminal, what should I do? 

[27186.400966] usb usb2-port1: Cannot enable. Maybe the USB cable is bad?
[27186.407581] usb usb2-port1: cannot disable (err = -32)
[27190.484963] usb usb2-port1: Cannot enable. Maybe the USB cable is bad?
[27190.491578] usb usb2-port1: cannot disable (err = -32)

 

Steve

0 Kudos
1 Solution
1 Reply