Hi ,
We are using custom board based on LS2088a RDB, in which we have only one USB3.0 port.
We can connect and use a usb3.0 devices successfully, but not able to detect the usb2.0 device either in u-boot or in kernel. Need your help to get the usb2.0 working.
Below are the logs.
root@localhost:~# [ 57.456745] usb usb1-port1: Cannot enable. Maybe the USB cable is bad?
[ 61.548745] usb usb1-port1: Cannot enable. Maybe the USB cable is bad?
[ 65.956739] usb usb1-port1: Cannot enable. Maybe the USB cable is bad?
Hello Pranav Shivalingaiah,
I have verified USB 2.0 device connecting to USB 3.0 port on LS2088ARDB with LSDK 1809 images, there is no problem, it worked normally.
Probably there is problem with USB cable, we have several USB cables, some can work, but some cannot.
Thanks,
Yiping