USB 2.0 3.0 OTG Serial Gadget LS1021A TWR Board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

USB 2.0 3.0 OTG Serial Gadget LS1021A TWR Board

843 Views
jiye
Contributor V

Hi,

 

I am trying to configure USB 2.0 (A) or USB3.0(B) as serial port on the eva board of LS1021ATWR. I know USB3.0 (B) has USB2.0 in it, and there is another USB2.0 (A) see Figure 2-9

I said USB2.0 as A here to indicate this is only USB2.0 controller not the USB2.0 in USB3.0

I said USB3.0 as B here to indicate USB3.0 controller which has both USB3.0 and USB2.0

Correct me if I am wrong

From the TWR-LS1021A reference manual. I found

pastedImage_2.png

pastedImage_1.png

Seems like if I want to use USB1 (USB3.0 which contains USB2.0) to achieve serial access I need to get rid of the HUB on the board? what if I need to use USB2 to achieve serial access.

I assume these two pins are either (D21 and D22)  or (D23 and D24) is USB 2.0 all I need to do is to connect the usb 2.0 cable wires (4 in total) , D+ and D- to these two pins.

Now question comes to what do I need to do to configure the USB 3.0 (B) or USB 2.0 (A) to serial port.

I already enabled necessary modules from the kconfig.

(1)what do I need to modify in the device tree file ?

the one @8600000 is USB1 or USB2 from Figure 2-9? It says host which is not the right mode for serial.

pastedImage_3.png

(2) what do I need to do to make USB3.0(B) acting like serial port?

(3) what do I need to do to make USB2.0(A) acting like serial port?

(4) if (2) is available how do I test it ?

Labels (1)
0 Kudos
7 Replies

681 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Elias Bitbaker,

It's impossible to use device (or Gadget) mode on LS1021ATWR, because there is a USB hub on this board.

If you want to use USB gadget, you could refer to the design of LS1021AQDS.

Thanks,

Yiping

0 Kudos

681 Views
jiye
Contributor V

also if I remove the USB hub from the LS1021a-TWR, can I use the USB gadget by connecting wires on the edge of the board D port ?

pastedImage_1.png

0 Kudos

681 Views
yipingwang
NXP TechSupport
NXP TechSupport

You could use USB gadget mode if removing USB hub in your design.

0 Kudos

681 Views
jiye
Contributor V

when you mention the usb hub are you talking about the U29 or the part U20B and U20C from the schematic 

0 Kudos

681 Views
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to the attached patch to Disable all USB3 ports on all root hubs and Power on USB2 root hub ports only.

0 Kudos

681 Views
jiye
Contributor V

(1) can I use the USB2.0 from the secondary pin connector D port on the edge of the board ? If so can i configure the usb2.0 as Ethernet gadget?

pastedImage_1.png

pastedImage_1.png

(2) is this picture above for USB2.0 ?

0 Kudos

681 Views
jiye
Contributor V

i can't find anything about LS1021AQDS, can you share me a link with this board's datasheet?

0 Kudos