I am trying to access the QSPI-NOR of the TWR-LS1021A-PB board (with a revision 2 silicon) using the sdcard-qspi u-boot build from the QorIQ SDK 2.0. When after booting from the SD card the u-boot command "sf probe" gives the following output:
U-Boot 2016.012.0+ga9b437f (Jul 21 2016 - 11:38:15 +0200)
CPU: Freescale LayerScape LS1021E, Version: 2.0, (0x87081120)
Clock Configuration:
CPU0(ARMV7):1000 MHz,
Bus:300 MHz, DDR:800 MHz (1600 MT/s data rate),
Reset Configuration Word (RCW):
00000000: 0608000a 00000000 00000000 00000000
00000010: 70000000 00007900 e0025a00 21046000
00000020: 00000000 00000000 00000000 20000000
00000030: 00080000 881b7340 00000000 00000000
I2C: ready
Model: LS1021A TWR Board
Board: LS1021ATWR
DRAM: 1 GiB
Using SERDES1 Protocol: 112 (0x70)
MMC: FSL_SDHC: 0
EEPROM: NXID v16777216
PCIe1: Root Complex no link, regs @ 0x3400000
PCIe2: Root Complex no link, regs @ 0x3500000
In: serial
Out: serial
Err: serial
SEC0: RNG instantiated
SATA link 0 timeout.
AHCI 0001.0300 1 slots 1 ports ? Gbps 0x1 impl SATA mode
flags: 64bit ncq pm clo only pmp fbss pio slum part ccc
Found 0 device(s).
SCSI: Net: eTSEC2 is in sgmii mode.
eTSEC1 [PRIME], eTSEC2, eTSEC3
=> sf probe
SF: Unsupported flash IDs: manuf 00, jedec 0000, ext_jedec 0000
Failed to initialize SPI flash at 0:0 (error -22)
I am using the following DIP switch settings:
SW2[1:8] = 00100111
SW3[1:8] = 01100101
After enabling debugging in the fsl_qspi.c driver and adding the following printf I get the following output:
int qspi_xfer(struct fsl_qspi_priv *priv, unsigned int bitlen,
const void *dout, void *din, unsigned long flags)
{
u32 bytes = DIV_ROUND_UP(bitlen, 8);
static u32 wr_sfaddr;
u32 txbuf;
printf("qspi_xfer:\nbitlen=0x%08x\nflags=0x%08x\nbus_clk=0x%08x\ncur_seqid=0x%08x\nspeed_hz=0x%08x\nsf_addr=0x%08x\nflash_num=0x%08x\nnum_chipselect=0x%08x\n",
bitlen, flags, priv->bus_clk, priv->cur_seqid, priv->speed_hz, priv->sf_addr, priv->flash_num, priv->num_chipselect);
if (dout) {
=> sf probe
fsl_qspi_ofdata_to_platdata: regs=<0x1550000> <0x40000000, 0x4000000>, max-frequency=50000000, endianess=be
qspi_xfer:
bitlen=0x00000008
flags=0x00000001
bus_clk=0x00000000
cur_seqid=0x00000000
speed_hz=0x02faf080
sf_addr=0x00000000
flash_num=0x00000001
num_chipselect=0x00000002
qspi_xfer:
bitlen=0x00000028
flags=0x00000002
bus_clk=0x00000000
cur_seqid=0x0000009f
speed_hz=0x02faf080
sf_addr=0x00000000
flash_num=0x00000001
num_chipselect=0x00000002
SF: Unsupported flash IDs: manuf 00, jedec 0000, ext_jedec 0000
Failed to initialize SPI flash at 0:0 (error -22)
Do I miss a configuration or does the SDK 2.0 have a known bug that can explain this behavior?