使用T2080的MAC9 SGMII模式直接连接BCM5396 port,能否正常连接,MAC9能否设置成1000base-kx模式。
> Using T2080's MAC9 SGMII mode to directly connect to the BCM5396.
> Can it be connected normally? Can MAC9 be set to 1000base-kx mode?
Yes, it can.
Please refer to the QorIQ T2080 Reference Manual, 19.6.1.2 1000Base-KX
好的,非常感谢,您知道BCM5396端口设置成什么模式,是SGMII模式还是SERDES模式?
Please communicate in English.