T2080的MAC9支持MACtoMAC的模式吗

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

T2080的MAC9支持MACtoMAC的模式吗

444 Views
735362573
Contributor I

使用T2080的MAC9 SGMII模式直接连接BCM5396 port,能否正常连接,MAC9能否设置成1000base-kx模式。

0 Kudos
3 Replies

371 Views
ufedor
NXP Employee
NXP Employee

> Using T2080's MAC9 SGMII mode to directly connect to the BCM5396.

> Can it be connected normally? Can MAC9 be set to 1000base-kx mode?

Yes, it can.

Please refer to the QorIQ T2080 Reference Manual, 19.6.1.2 1000Base-KX

0 Kudos

371 Views
735362573
Contributor I

好的,非常感谢,您知道BCM5396端口设置成什么模式,是SGMII模式还是SERDES模式?

0 Kudos

371 Views
ufedor
NXP Employee
NXP Employee

Please communicate in English.

0 Kudos