Some problems about compile imx-android-p9.0.0_2.2.0-ga BSP

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Some problems about compile imx-android-p9.0.0_2.2.0-ga BSP

1,437 Views
946846828
Contributor II

Hi:

Followed the introduction of community: Downloading and Compiling Android9.0.0-2.0.0 BSP on Ubuntu16.04.2 LTS 

I used Vmware 12 and Ubuntu 16.04 LTS to test and check these contents step by step, but still met some problems when i do the operation: source ~/imx-p9.0.0_2.0.0-ga/imx_android_setup.sh,

The failure has been reported like: Could not resolve host: source.codeaurora.org.

it also reminded:  Python 2 is no longer supported; Please upgrade to Python 3.6+.

"repo sync" again also can not help, could you guys please help check them and give me some guides?

compiling issue.png

Labels (2)
0 Kudos
Reply
2 Replies

1,345 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello chu zhongbo,

Please put this problem in i.MX Processors .

Thanks,

Yiping

0 Kudos
Reply

1,345 Views
946846828
Contributor II

Sorry, i have changed it.

0 Kudos
Reply