Set Custom Hostname in LLDP SDK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Set Custom Hostname in LLDP SDK

282 Views
pvsnsubhash
Contributor II

I want to change the hostname of the LLDP SDK for NXP LX2160ARBD Board. I tried using "hostname" and "hostname_pn-base-files" in local.conf, but after building it shows the default hostname. I even tried creating a base-files recipe with a bbappend to modify hostname and hosts file in my custom layer, even that didn't work.. What else can be done?

 

Thanks and Regards
PVSN Subhash
0 Kudos
Reply
1 Reply

246 Views
June_Lu
NXP TechSupport
NXP TechSupport

If you want to add custom machine in the yocto, you could refer to

https://docs.nxp.com/bundle/UG10081_LLDP_L6.1.55_2.2.0/page/topics/how_to_add_a_custom_machine_in_fl...

Thanks

0 Kudos
Reply