SODIMM DDR is failing with LS1046ardb based custom board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SODIMM DDR is failing with LS1046ardb based custom board

499 Views
RatanLal
Contributor I

Hi 

 

We have made our custom board(with SODIMM - MTA9ASF2G72HZ-3G2F1) based on LS1046ardb(with DIMM - MTA18ASF1G72AZ-2G3B1)

when we are booting with our custom board we are getting below error logs 

 

NOTICE: UDIMM 9ASF2G72HZ-3G2F1
ERROR: Board parameters no match.
ERROR: Failed matching board timing.
ERROR: Found training error(s): 0x2100
ERROR: Error: Waiting for D_INIT timeout.
ERROR: Writing DDR register(s) failed
ERROR: Programing DDRC error
ERROR: DDR init failed.
NOTICE: Incorrect DRAM0 size is defined in platform_def.h
ERROR: mmap_add_region_check() failed. error -22
ERROR: mmap_add_region_check() failed. error -22
NOTICE: BL2: v2.4(release):la1224rdb-bsp1.9.0_p1-0-g682906eb7
NOTICE: BL2: Built : 12:07:18, Apr 14 2022

 

Please suggest for the same.

Labels (2)
Tags (2)
0 Kudos
0 Replies