SERDES GEN 3 Speeds

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SERDES GEN 3 Speeds

1,353 Views
vanlandingham10
Contributor II

The Ref man states that:

"PCIe Gen 3 speed support requires switching to second PLL so when Gen 3 is used
both SerDes PLL will be used by PCIe protocol."

 

Does this mean if I intend on using config 5577 for SERDES PORT 2 That I need to provide two separate external 100 MHZ refclks or can I just provide 1 external 100 MHz refclk and configure the internal mux to re-direct the 2nd pll to use the same external refclk?

 

0 Kudos
Reply
6 Replies

1,347 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @vanlandingham10 

Which specific processor are you referring to?

Regards,
Mrudang Shelat

 

0 Kudos
Reply

1,340 Views
vanlandingham10
Contributor II

sorry the LS1046

0 Kudos
Reply

1,352 Views
vanlandingham10
Contributor II

I'd like to configure the SERDES ports to support 5577 and 1133. Will my clock scheme work?

 

vanlandingham10_0-1665003409286.jpeg

 

0 Kudos
Reply

1,332 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi @vanlandingham10,

 

The clocking scheme looks fine.

 

Regards,
Mrudang Shelat

0 Kudos
Reply

1,317 Views
vanlandingham10
Contributor II

Okay so If SERDES2 is entirely used for pcie gen3 I can pass a single reference clock to each pll via the internal mux ?

0 Kudos
Reply

1,269 Views
mrudangshelat-13
NXP TechSupport
NXP TechSupport

Hi

 

Yes, you can configure SD2_REF_CLK1/SD2_REF_CLK1_B to both the PLL.

 

Regards,
Mrudang Shelat

0 Kudos
Reply