The Ref man states that:
"PCIe Gen 3 speed support requires switching to second PLL so when Gen 3 is used
both SerDes PLL will be used by PCIe protocol."
Does this mean if I intend on using config 5577 for SERDES PORT 2 That I need to provide two separate external 100 MHZ refclks or can I just provide 1 external 100 MHz refclk and configure the internal mux to re-direct the 2nd pll to use the same external refclk?
sorry the LS1046
I'd like to configure the SERDES ports to support 5577 and 1133. Will my clock scheme work?
Okay so If SERDES2 is entirely used for pcie gen3 I can pass a single reference clock to each pll via the internal mux ?
Hi
Yes, you can configure SD2_REF_CLK1/SD2_REF_CLK1_B to both the PLL.
Regards,
Mrudang Shelat