SDK v2.0-1701 PPA Build Failing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDK v2.0-1701 PPA Build Failing

Jump to solution
2,403 Views
vbonduro
Contributor II

Hello,

We're experiencing difficulties building fsl-image-core in SDK V2.0-1701. We can build in 1609 and 1611 just fine, but 1701 always fails building the ppa. We are experiencing the same issue on two systems, so it is not isolated to one environment.

I have tried wiping out my SDK directory and reinstalling SDK 2.0 & 1701 update again with no success. I have also tried re-downloading the 1701 update and I have verified that the MD5 of my download is valid.

Below are the steps I took when upgrading to 1701:

rm -rf src/local/QorIQ-SDK-V2.0-20160527-yocto

sudo mount -o loop QorIQ\ Linux\ SDK\ v2.0\ SOURCE.iso /mnt/cdrom

/mnt/cdrom/install

tar xjf SDK-V2.0-1701.tar.bz2

SDK-V2.0-1701/install

cd src/local/QorIQ-SDK-V2.0-20160527-yocto

./sources/meta-freescale/scripts/host-prepare.sh

. ./fsl-setup-env -m ls1043ardb

Here is a log of the failed build attempt. We receive the same error from bitbake fsl-image-core and when building only the ppa with: bitbake -c cleansstate ppa; bitbake -c patch ppa; bitbake -c compile -f ppa

Loading cache: 100% |#########################################################################################################################################################| ETA: 00:00:00
Loaded 3428 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.28.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Debian-8.5"
TARGET_SYS = "aarch64-fsl-linux"
MACHINE = "ls1043ardb"
DISTRO = "fsl-qoriq"
DISTRO_VERSION = "2.0"
TUNE_FEATURES = "aarch64"
TARGET_FPU = ""
meta
meta-yocto
meta-yocto-bsp = "HEAD:9a211a4a2c1bfcb292dc97d8dcac149bca9e3f1b"
meta-oe
meta-multimedia
meta-gnome
meta-networking
meta-perl
meta-python
meta-ruby
meta-filesystems
meta-webserver
meta-xfce = "HEAD:dc5634968b270dde250690609f0015f881db81f2"
meta-freescale = "HEAD:7facbdb726e2dda0515e084c2066a4b8dd99c6d2"
meta-freescale-internal = "HEAD:4829293f807e35a1111e79763294fc8b98b97810"
meta-freescale-extra = "HEAD:bee911b027e0480b034674d0ddee3fcb06d2e985"
meta-virtualization = "HEAD:042425c1d98bdd7e44a62789bd03b375045266f5"
meta-java = "HEAD:8b776ac68f9af4596be3824152bcf0bc6b67fa1d"
meta-openstack
meta-openstack-aio-deploy
meta-openstack-compute-deploy
meta-openstack-compute-test-config
meta-openstack-controller-deploy
meta-openstack-controller-test-config
meta-openstack-qemu
meta-openstack-swift-deploy
meta-cloud-services = "HEAD:d8bc0d92d0f741e2ea1e6d3d9bc6b7a091d03cfb"
meta-security = "HEAD:f9367e71f923fc7d2fb600208e2b97535ea41777"
meta-linaro-toolchain = "HEAD:10b71bed9cfe76baa22c72806ff814cf85c2f73b"
meta-nxp-npi-1701 = "jethro-sdk-v2.0-ga-1701:11975eebce9096a3567d00ba2067a2dbd2ed4d5c"

NOTE: Preparing RunQueue
NOTE: Tainting hash to force rebuild of task /home/vincentbonduro/src/local/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-bsp/ppa/ppa_git.bb, do_compile
WARNING: /home/vincentbonduro/src/local/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-bsp/ppa/ppa_git.bb.do_compile is tainted from a forced run
NOTE: Checking sstate mirror object availability (for 32 objects)
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: oe_runmake failed
ERROR: Function failed: do_compile (log file is located at /home/vincentbonduro/src/local/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/aarch64-fsl-linux/ppa/git-r0/temp/log.do_compile.404)
ERROR: Logfile of failure stored in: /home/vincentbonduro/src/local/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/aarch64-fsl-linux/ppa/git-r0/temp/log.do_compile.404
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make CC64=aarch64-fsl-linux-gcc --sysroot=/home/vincentbonduro/src/local/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/sysroots/ls1043ardb LD64=aarch64-fsl-linux-ld --sysroot=/home/vincentbonduro/src/local/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/sysroots/ls1043ardb OBJ64=aarch64-fsl-linux-objcopy rdb-fit
| build: image=fit \ gicv2 \ cci400 \ debug off \ test ""
|
| aarch64-fsl-linux-gcc --sysroot=/home/vincentbonduro/src/local/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/sysroots/ls1043ardb -Wl,-O1 -Wl,--hash-style=gnu -Wl,--as-needed -o .o
| /home/vincentbonduro/src/local/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/sysroots/ls1043ardb/usr/lib/../lib/crt1.o: In function `_start':
| /home/vincentbonduro/src/local/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/aarch64-fsl-linux/glibc/linaro-2.20-r2014.11/glibc-linaro-2.20-2014.11/csu/../sysdeps/aarch64/start.S:87: undefined reference to `main'
| collect2: error: ld returned 1 exit status
| <builtin>: recipe for target '.o' failed
| make[1]: *** [.o] Error 1
| plat.mk:26: recipe for target 'rdb-fit' failed
| make: *** [rdb-fit] Error 2
| WARNING: exit code 1 from a shell command.
| ERROR: oe_runmake failed
| ERROR: Function failed: do_compile (log file is located at /home/vincentbonduro/src/local/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/aarch64-fsl-linux/ppa/git-r0/temp/log.do_compile.404)
ERROR: Task 4 (/home/vincentbonduro/src/local/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-bsp/ppa/ppa_git.bb, do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 240 tasks of which 196 didn't need to be rerun and 1 failed.

Summary: 1 task failed:
/home/vincentbonduro/src/local/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-bsp/ppa/ppa_git.bb, do_compile
Summary: There was 1 WARNING message shown.
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

I removed my QorIQ-SDK-V2.0-20160527-yocto directory and reinstalled SDK 2.0 with 1609 and the build started working again.

Both systems are running Debian Jessie:

vincentbonduro@debian:~/Downloads$ cat /etc/os-release
PRETTY_NAME="Debian GNU/Linux 8 (jessie)"
NAME="Debian GNU/Linux"
VERSION_ID="8"
VERSION="8 (jessie)"
ID=debian
HOME_URL="http://www.debian.org/"
SUPPORT_URL="http://www.debian.org/support"
BUG_REPORT_URL="https://bugs.debian.org/"


vincentbonduro@debian:~/Downloads$ uname -a
Linux debian 3.16.0-4-amd64 #1 SMP Debian 3.16.7-ckt25-2 (2016-04-08) x86_64 GNU/Linux

Labels (1)
1 Solution
1,417 Views
yipingwang
NXP TechSupport
NXP TechSupport

I have tried to reproduce the issue, the issue appears when make-4.1 is used. Build can pass when make-3.81 is used.  Seems the ppa Makefile should be fixed to be compatible with new make utility. The workaround is to install make-3.81 on host and use the old make to compile.



Have a great day,
Yiping

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

4 Replies
1,417 Views
yipingwang
NXP TechSupport
NXP TechSupport

Hello Vincent Bonduro,

According to the error log, it looks there is problem with glibc libs to cause the link error.

Please rebuild glibc with the following commands, then check whether PPA could be built successfully.

$ bitbake glibc -c cleansstate

$ bitbake glibc

If the problem remains, please feel free to let me know.


Have a great day,
Yiping

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
1,417 Views
vbonduro
Contributor II

Hi Yiping,

Thanks for the reply!

Unfortunately, it appears PPA is still failing even after buidling glibc. Logs are below:

vincentbonduro@debian:~/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb$ bitbake glibc -c cleansstate
Parsing recipes: 100% |########################################################################################################| Time: 00:21:46
Parsing of 2722 .bb files complete (0 cached, 2722 parsed). 3427 targets, 250 skipped, 5 masked, 0 errors.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.28.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Debian-8.5"
TARGET_SYS = "aarch64-fsl-linux"
MACHINE = "ls1043ardb"
DISTRO = "fsl-qoriq"
DISTRO_VERSION = "2.0"
TUNE_FEATURES = "aarch64"
TARGET_FPU = ""
meta
meta-yocto
meta-yocto-bsp = "HEAD:9a211a4a2c1bfcb292dc97d8dcac149bca9e3f1b"
meta-oe
meta-multimedia
meta-gnome
meta-networking
meta-perl
meta-python
meta-ruby
meta-filesystems
meta-webserver
meta-xfce = "HEAD:dc5634968b270dde250690609f0015f881db81f2"
meta-freescale = "HEAD:7facbdb726e2dda0515e084c2066a4b8dd99c6d2"
meta-freescale-internal = "HEAD:4829293f807e35a1111e79763294fc8b98b97810"
meta-freescale-extra = "HEAD:bee911b027e0480b034674d0ddee3fcb06d2e985"
meta-virtualization = "HEAD:042425c1d98bdd7e44a62789bd03b375045266f5"
meta-java = "HEAD:8b776ac68f9af4596be3824152bcf0bc6b67fa1d"
meta-openstack
meta-openstack-aio-deploy
meta-openstack-compute-deploy
meta-openstack-compute-test-config
meta-openstack-controller-deploy
meta-openstack-controller-test-config
meta-openstack-qemu
meta-openstack-swift-deploy
meta-cloud-services = "HEAD:d8bc0d92d0f741e2ea1e6d3d9bc6b7a091d03cfb"
meta-security = "HEAD:f9367e71f923fc7d2fb600208e2b97535ea41777"
meta-linaro-toolchain = "HEAD:10b71bed9cfe76baa22c72806ff814cf85c2f73b"
meta-nxp-npi-1701 = "jethro-sdk-v2.0-ga-1701:11975eebce9096a3567d00ba2067a2dbd2ed4d5c"

NOTE: Preparing RunQueue
NOTE: Executing RunQueue Tasks
NOTE: Tasks Summary: Attempted 2 tasks of which 0 didn't need to be rerun and all succeeded.
vincentbonduro@debian:~/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb$ bitbake glibc
Loading cache: 100% |##########################################################################################################| ETA: 00:00:00
Loaded 3428 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.28.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Debian-8.5"
TARGET_SYS = "aarch64-fsl-linux"
MACHINE = "ls1043ardb"
DISTRO = "fsl-qoriq"
DISTRO_VERSION = "2.0"
TUNE_FEATURES = "aarch64"
TARGET_FPU = ""
meta
meta-yocto
meta-yocto-bsp = "HEAD:9a211a4a2c1bfcb292dc97d8dcac149bca9e3f1b"
meta-oe
meta-multimedia
meta-gnome
meta-networking
meta-perl
meta-python
meta-ruby
meta-filesystems
meta-webserver
meta-xfce = "HEAD:dc5634968b270dde250690609f0015f881db81f2"
meta-freescale = "HEAD:7facbdb726e2dda0515e084c2066a4b8dd99c6d2"
meta-freescale-internal = "HEAD:4829293f807e35a1111e79763294fc8b98b97810"
meta-freescale-extra = "HEAD:bee911b027e0480b034674d0ddee3fcb06d2e985"
meta-virtualization = "HEAD:042425c1d98bdd7e44a62789bd03b375045266f5"
meta-java = "HEAD:8b776ac68f9af4596be3824152bcf0bc6b67fa1d"
meta-openstack
meta-openstack-aio-deploy
meta-openstack-compute-deploy
meta-openstack-compute-test-config
meta-openstack-controller-deploy
meta-openstack-controller-test-config
meta-openstack-qemu
meta-openstack-swift-deploy
meta-cloud-services = "HEAD:d8bc0d92d0f741e2ea1e6d3d9bc6b7a091d03cfb"
meta-security = "HEAD:f9367e71f923fc7d2fb600208e2b97535ea41777"
meta-linaro-toolchain = "HEAD:10b71bed9cfe76baa22c72806ff814cf85c2f73b"
meta-nxp-npi-1701 = "jethro-sdk-v2.0-ga-1701:11975eebce9096a3567d00ba2067a2dbd2ed4d5c"

NOTE: Preparing RunQueue
NOTE: Checking sstate mirror object availability (for 148 objects)
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
NOTE: Tasks Summary: Attempted 600 tasks of which 336 didn't need to be rerun and all succeeded.
vincentbonduro@debian:~/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb$ bitbake fsl-image-core
Loading cache: 100% |##########################################################################################################| ETA: 00:00:00
Loaded 3428 entries from dependency cache.
NOTE: Resolving any missing task queue dependencies

Build Configuration:
BB_VERSION = "1.28.0"
BUILD_SYS = "x86_64-linux"
NATIVELSBSTRING = "Debian-8.5"
TARGET_SYS = "aarch64-fsl-linux"
MACHINE = "ls1043ardb"
DISTRO = "fsl-qoriq"
DISTRO_VERSION = "2.0"
TUNE_FEATURES = "aarch64"
TARGET_FPU = ""
meta
meta-yocto
meta-yocto-bsp = "HEAD:9a211a4a2c1bfcb292dc97d8dcac149bca9e3f1b"
meta-oe
meta-multimedia
meta-gnome
meta-networking
meta-perl
meta-python
meta-ruby
meta-filesystems
meta-webserver
meta-xfce = "HEAD:dc5634968b270dde250690609f0015f881db81f2"
meta-freescale = "HEAD:7facbdb726e2dda0515e084c2066a4b8dd99c6d2"
meta-freescale-internal = "HEAD:4829293f807e35a1111e79763294fc8b98b97810"
meta-freescale-extra = "HEAD:bee911b027e0480b034674d0ddee3fcb06d2e985"
meta-virtualization = "HEAD:042425c1d98bdd7e44a62789bd03b375045266f5"
meta-java = "HEAD:8b776ac68f9af4596be3824152bcf0bc6b67fa1d"
meta-openstack
meta-openstack-aio-deploy
meta-openstack-compute-deploy
meta-openstack-compute-test-config
meta-openstack-controller-deploy
meta-openstack-controller-test-config
meta-openstack-qemu
meta-openstack-swift-deploy
meta-cloud-services = "HEAD:d8bc0d92d0f741e2ea1e6d3d9bc6b7a091d03cfb"
meta-security = "HEAD:f9367e71f923fc7d2fb600208e2b97535ea41777"
meta-linaro-toolchain = "HEAD:10b71bed9cfe76baa22c72806ff814cf85c2f73b"
meta-nxp-npi-1701 = "jethro-sdk-v2.0-ga-1701:11975eebce9096a3567d00ba2067a2dbd2ed4d5c"

NOTE: Preparing RunQueue
NOTE: Checking sstate mirror object availability (for 759 objects)
NOTE: Executing SetScene Tasks
NOTE: Executing RunQueue Tasks
ERROR: oe_runmake failed
ERROR: Function failed: do_compile (log file is located at /home/vincentbonduro/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/aarch64-fsl-linux/ppa/git-r0/temp/log.do_compile.8452)
ERROR: Logfile of failure stored in: /home/vincentbonduro/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/aarch64-fsl-linux/ppa/git-r0/temp/log.do_compile.8452
Log data follows:
| DEBUG: Executing shell function do_compile
| NOTE: make CC64=aarch64-fsl-linux-gcc --sysroot=/home/vincentbonduro/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/sysroots/ls1043ardb LD64=aarch64-fsl-linux-ld --sysroot=/home/vincentbonduro/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/sysroots/ls1043ardb OBJ64=aarch64-fsl-linux-objcopy rdb-fit
| build: image=fit \ gicv2 \ cci400 \ debug off \ test ""
|
| aarch64-fsl-linux-gcc --sysroot=/home/vincentbonduro/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/sysroots/ls1043ardb -Wl,-O1 -Wl,--hash-style=gnu -Wl,--as-needed -o .o
| /home/vincentbonduro/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/sysroots/ls1043ardb/usr/lib/../lib/crt1.o: In function `_start':
| /home/vincentbonduro/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/aarch64-fsl-linux/glibc/linaro-2.20-r2014.11/glibc-linaro-2.20-2014.11/csu/../sysdeps/aarch64/start.S:87: undefined reference to `main'
| collect2: error: ld returned 1 exit status
| <builtin>: recipe for target '.o' failed
| make[1]: *** [.o] Error 1
| plat.mk:26: recipe for target 'rdb-fit' failed
| make: *** [rdb-fit] Error 2
| WARNING: exit code 1 from a shell command.
| ERROR: oe_runmake failed
| ERROR: Function failed: do_compile (log file is located at /home/vincentbonduro/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/aarch64-fsl-linux/ppa/git-r0/temp/log.do_compile.8452)
ERROR: Task 118 (/home/vincentbonduro/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-bsp/ppa/ppa_git.bb, do_compile) failed with exit code '1'
NOTE: Tasks Summary: Attempted 2057 tasks of which 936 didn't need to be rerun and 1 failed.
Waiting for 0 running tasks to finish:

Summary: 1 task failed:
/home/vincentbonduro/QorIQ-SDK-V2.0-20160527-yocto/sources/meta-freescale/recipes-bsp/ppa/ppa_git.bb, do_compile
Summary: There were 2 ERROR messages shown, returning a non-zero exit code.

0 Kudos
1,417 Views
perdalen
Contributor III

I have the same problem.

Do anyone from support have any solution of this problem?

Thanks

0 Kudos
1,418 Views
yipingwang
NXP TechSupport
NXP TechSupport

I have tried to reproduce the issue, the issue appears when make-4.1 is used. Build can pass when make-3.81 is used.  Seems the ppa Makefile should be fixed to be compatible with new make utility. The workaround is to install make-3.81 on host and use the old make to compile.



Have a great day,
Yiping

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------