SD card image for the ls1046ardb with yocto and WIC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SD card image for the ls1046ardb with yocto and WIC

1,252 Views
andreyrafalsky
Contributor III

Hi,

I need to create sd card image for the ls1046ardb with wic or similar tools.

Now I can manually deploy image to the sd card by guide from the QorIQ LS1046A BSP v0.4. It works but I need to use the automatic deployment method.

I tried to use wic but it creates the wrong image. It seems to me that I have some issue with preparation of the wks file.

Advise me please wks file content for sd card image. Also any information about the automatic deployment method will be greatly valuable for me.

Thank

Andrey

Labels (1)
0 Kudos
2 Replies

896 Views
Pavel
NXP Employee
NXP Employee

Look at the Section 4.4.8.9.4 of SDK 2.0-1703 documentation:

https://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf

 

See also the Section 4.1.2 of LSDK documentation:

https://www.nxp.com/docs/en/supporting-information/LSDK-KC-REV18.03.pdf

 

These documentations contain command sequence for SD card image deployment.

Use this command sequence for SD card image deployment.


Have a great day,
Pavel Chubakov

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

894 Views
andreyrafalsky
Contributor III

Hi Pavel,

Thank for your reply.

I created SD card image with wic.

Best regards,

Andrey

0 Kudos