SD Card Boot for LS1043A failing in BL2 (DDR4 issue?)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SD Card Boot for LS1043A failing in BL2 (DDR4 issue?)

2,113 Views
ssreeraj
Contributor I

We have designed a custom board using LS1043A based on the LS1043ARDB reference design. We have 4GB of DDR4, using 4 x MT40A1G8SA-075:E, clocked at 800 MHz (1600 DDR). The RCW used and relevant parts of the atf/plat/nxp/soc-ls1043/ls1043ardb/ddr_init.c is given further below.

Notes:

1. Clocking is derived from differential SYSCLK inputs which is 100 MHz

2. SD Card boot image (not secure boot) is build with “flex-builder -i mksw -m ls1043ardb -b sd”

 

Booting from SD card progresses till loading of next stage where the BL3 never starts. The console stops at the following point:

INFO: BL2: Doing platform setup

INFO: BL2: Loading image id 3

INFO: sd-mmc read done.

We believe that this could be due to errors on the DDR. We are looking for help in what needs to be modified in order to get it to the uboot prompt. We have the following observations and queries in this regard:

1. We have bit swizzling within each nibble and accordingly we changed the DQ pin mapping in ddr_raw_timing variable in file ddr_init.c. Till we changed this to the correct values based on the bit swizzling on our board (Relevant parts of the schematics attached), the BL2 compiled with DDR_DEBUG=yes, DDR_BIST=yes and DEBUG=1 was reporting “Error in training” and “DDR init failed” messages. But now we are not getting these errors (see boot log below). It even reports “Built-in self-test passed” message, although there is a “time out” error – see output on console below:

INFO: Running built-in self test ...

INFO: Wait up to 3300 ms

ERROR: Timeout

NOTICE: Build-in self test passed

 

QUERY: Does the above mean that the DDR is working properly? If so what other reason could be there for the boot to fail? Note that the same code with just the bit-swizzling (DQ map settings) corrected to have no swizzliing boots in the LS1043ARDB reference design board.

2. We also changed the rank_density and capacity to 4294967296u for 4GB in the struct dimm_params along with increasing n_row_addr to 16 (15 in RDB with 2 GB DDR), but retained n_ranks=1 and bank_group_bits = 2.

QUERY: Is this ok?

3. The timing configuration variables were modified based on the DDR part’s datasheet. These modified timings were verified to work in RDB as the part used in RDB has very similar timings. But we did not modify the “struct rc_timing rcz” and “struct board_timing ram[]” from their values for RDB as we do not know what these parameters mean.

QUERY: Should we be changing rcz and ram[] variables? Any documentation on these?

4. We did not modify anything in the ddr_board_options() function.

QUERY: Any changes required here?

5. QUERY: Any issue in the schematics attached?

6. QUERY: Anything else we can try out to fix the issue?

 

ddr_init.c File

struct dimm_params ddr_raw_timing = { //MODIFIED

.n_ranks = 1,

.rank_density = 4294967296u, //MODIFIED

.capacity = 4294967296u, //MODIFIED

.primary_sdram_width = 32,

.rdimm = 0,

.mirrored_dimm = 0,

.n_row_addr = 16, //MODIFIED

.n_col_addr = 10,

.bank_group_bits = 2,

.edc_config = 0,

.burst_lengths_bitmask = 0x0c,

.tckmin_x_ps = 938,

.tckmax_ps = 1500,

.caslat_x = 0x0001FFE00, //MODIFIED

.dq_mapping[0] = 0x00,

.dq_mapping[1] = 0x21, //MODIFIED

.dq_mapping[2] = 0x16, //MODIFIED

.dq_mapping[3] = 0x35, //MODIFIED

.dq_mapping[4] = 0x16, //MODIFIED

.dq_mapping[5] = 0x36, //MODIFIED

.dq_mapping[6] = 0x08, //MODIFIED

.dq_mapping[7] = 0x36, //MODIFIED

.dq_mapping[8] = 0x0,

.dq_mapping[9] = 0x0,

.dq_mapping[10] = 0x0,

.dq_mapping[11] = 0x0,

.dq_mapping[12] = 0x0,

.dq_mapping[13] = 0x0,

.dq_mapping[14] = 0x0,

.dq_mapping[15] = 0x0,

.dq_mapping[16] = 0x0,

.dq_mapping[17] = 0x0,

.dq_mapping_ors = 0,

.taa_ps = 14250, //MODIFIED

.trcd_ps = 14250, //MODIFIED

.trp_ps = 14250, //MODIFIED

.tras_ps = 32000, //MODIFIED

.trc_ps = 46250, //MODIFIED

.twr_ps = 15000,

.trfc1_ps = 350000, //MODIFIED

.trfc2_ps = 260000, //MODIFIED

.trfc4_ps = 160000, //MODIFIED

.tfaw_ps = 25000, //MODIFIED

.trrds_ps = 5000, //MODIFIED

.trrdl_ps = 5000, //MODIFIED

.tccdl_ps = 5000, //MODIFIED

.refresh_rate_ps = 7800000,

.rc = 0x1f,

};

 

static const struct rc_timing rcz[] = { //NOT MODIFIED FROM RDB

{1600, 12, 7},

{}

};

 

static const struct board_timing ram[] = { //NOT MODIFIED FROM RDB

{0x1f, rcz, 0x00020100, 0},

};

 

int ddr_board_options(struct ddr_info *priv) //NOT MODIFIED FROM RDB

{

int ret;

struct memctl_opt *popts = &priv->opt;

 

ret = cal_board_params(priv, ram, ARRAY_SIZE(ram));

if (ret)

return ret;

popts->cpo_sample = 0x46;

popts->ddr_cdr1 = DDR_CDR1_DHC_EN |

DDR_CDR1_ODT(DDR_CDR_ODT_80ohm);

popts->ddr_cdr2 = DDR_CDR2_ODT(DDR_CDR_ODT_80ohm) |

DDR_CDR2_VREF_OVRD(70); /* Vref = 70% */

return 0;

}

 

RCW settings

SYS_PLL_RAT=4

MEM_PLL_RAT=16

CGA_PLL1_RAT=16

CGA_PLL2_RAT=10

SRDS_PRTCL_S1=13144

FM1_MAC_RAT=1

SRDS_PLL_REF_CLK_SEL_S1=0

SRDS_DIV_PEX=1

DDR_FDBK_MULT=2

DDR_REFCLK_SEL=1

PBI_src=6

IFC_MODE=37

HWA_CGA_M1_CLK_SEL=6

DRAM_LAT=1

SYS_PLL_SPD=1

UART_EXT=0

IRQ_EXT=0

SPI_EXT=0

SDHC_EXT=0

UART_BASE=5

SDHC_BASE=0

IRQ_OUT=1

IRQ_BASE=1

SPI_BASE=0

EC1=0

EC2=0

EM1=0

EM2=0

EMI2_DMODE=1

EMI2_CMODE=1

TVDD_VSEL=1

DVDD_VSEL=2

QE_CLK_OVRRIDE=0

EMI1_DMODE=1

EVDD_VSEL=2

IIC2_BASE=0

EMI1_CMODE=1

IIC2_EXT=0

SYSCLK_FREQ=600

HWA_CGA_M2_CLK_SEL=1

 

=====================================

 

Boot Console Log: (Hangs before loading next stage)

 

=====================================

 

INFO: SoC workaround for Errata A008850 Early-Phase was applied

INFO: SoC workaround for Errata A009660 was applied

INFO: SoC workaround for Errata A010539 was applied

INFO: RCW BOOT SRC is SD/EMMC

INFO: SoC workaround for DDR Errata A009942 was applied

INFO: SoC workaround for DDR Errata A009663 was applied

NOTICE: platform clock 400000000

NOTICE: DDR PLL1 1600000000

NOTICE: DDR PLL2 400000000

INFO: time base 8 ms

INFO: Parse DIMM SPD(s)

INFO: cs_in_use = 1

INFO: cs_on_dimm[0] = 1

NOTICE: Fixed DDR on board

INFO: Time after parsing SPD 14 ms

INFO: Synthesize configurations

INFO: cs 0

INFO: odt_rd_cfg 0x0

INFO: odt_wr_cfg 0x4

INFO: odt_rtt_norm 0x3

INFO: odt_rtt_wr 0x0

INFO: auto_precharge 0

INFO: cs 1

INFO: odt_rd_cfg 0x0

INFO: odt_wr_cfg 0x0

INFO: odt_rtt_norm 0x0

INFO: odt_rtt_wr 0x0

INFO: auto_precharge 0

INFO: cs 2

INFO: odt_rd_cfg 0x0

INFO: odt_wr_cfg 0x0

INFO: odt_rtt_norm 0x0

INFO: odt_rtt_wr 0x0

INFO: auto_precharge 0

INFO: cs 3

INFO: odt_rd_cfg 0x0

INFO: odt_wr_cfg 0x0

INFO: odt_rtt_norm 0x0

INFO: odt_rtt_wr 0x0

INFO: auto_precharge 0

INFO: ctlr_init_ecc 0

INFO: x4_en 0

INFO: ap_en 0

INFO: ctlr_intlv 0

INFO: ctlr_intlv_mode 0

INFO: ba_intlv 0x0

INFO: data_bus_used 1

INFO: otf_burst_chop_en 0

INFO: burst_length 0x8

INFO: dbw_cap_shift 0

INFO: Assign binding addresses

INFO: ctlr_intlv 0

INFO: rank density 0x100000000

INFO: CS 0

INFO: base_addr 0x0

INFO: size 0x100000000

INFO: base 0x0

INFO: Total mem by assignment is 0x100000000

INFO: Calculate controller registers

INFO: Skip CL mask for this speed 0x0

INFO: Skip caslat 0x0

INFO: cal cs

INFO: cs_in_use = 0x1

INFO: cs0

INFO: _config = 0x80040322

INFO: cs[0].bnds = 0xff

INFO: sdram_cfg[0] = 0xc50c0000

INFO: sdram_cfg[1] = 0x401100

INFO: sdram_cfg[2] = 0x0

INFO: timing_cfg[0] = 0x91550018

INFO: timing_cfg[1] = 0xcac60c42

INFO: timing_cfg[2] = 0x48c114

INFO: timing_cfg[3] = 0x1111000

INFO: timing_cfg[4] = 0x2

INFO: timing_cfg[5] = 0x4401400

INFO: timing_cfg[6] = 0x0

INFO: timing_cfg[7] = 0x23300000

INFO: timing_cfg[8] = 0x3114600

INFO: timing_cfg[9] = 0x0

INFO: dq_map[0] = 0x215b558

INFO: dq_map[1] = 0xd88d8000

INFO: dq_map[2] = 0x0

INFO: dq_map[3] = 0x0

INFO: sdram_mode[0] = 0x3010214

INFO: sdram_mode[1] = 0x0

INFO: sdram_mode[9] = 0x4000000

INFO: sdram_mode[8] = 0x500

INFO: sdram_mode[2] = 0x10214

INFO: sdram_mode[3] = 0x0

INFO: sdram_mode[10] = 0x400

INFO: sdram_mode[11] = 0x4000000

INFO: sdram_mode[4] = 0x10214

INFO: sdram_mode[5] = 0x0

INFO: sdram_mode[12] = 0x400

INFO: sdram_mode[13] = 0x4000000

INFO: sdram_mode[6] = 0x10214

INFO: sdram_mode[7] = 0x0

INFO: sdram_mode[14] = 0x400

INFO: sdram_mode[15] = 0x4000000

INFO: interval = 0x18600618

INFO: zq_cntl = 0x8a090705

INFO: ddr_sr_cntr = 0x0

INFO: clk_cntl = 0x2000000

INFO: cdr[0] = 0x80040000

INFO: cdr[1] = 0xa181

INFO: wrlvl_cntl[0] = 0x8675f605

INFO: wrlvl_cntl[1] = 0x6070705

INFO: wrlvl_cntl[2] = 0x5050508

INFO: debug[28] = 0x46

INFO: Time before programming controller 262 ms

INFO: Program controller registers

INFO: Reading debug[9] as 0x16001600

INFO: Reading debug[10] as 0x1a001c00

INFO: cpo_min 0x16

INFO: cpo_max 0x1c

INFO: debug[28] 0x700046

INFO: Optimal cpo_sample 0x40

INFO: Running built-in self test ...

INFO: Wait up to 3300 ms

ERROR: Timeout

NOTICE: Build-in self test passed

INFO: *0x1080000 = 0xff

INFO: *0x1080080 = 0x80040322

INFO: *0x1080100 = 0x1111000

INFO: *0x1080104 = 0x91550018

INFO: *0x1080108 = 0xcac60c42

INFO: *0x108010c = 0x48c114

INFO: *0x1080110 = 0xc50c0000

INFO: *0x1080114 = 0x401100

INFO: *0x1080118 = 0x3010214

INFO: *0x1080124 = 0x18600618

INFO: *0x1080128 = 0xdeadbeef

INFO: *0x1080130 = 0x2000000

INFO: *0x1080160 = 0x2

INFO: *0x1080164 = 0x4401400

INFO: *0x108016c = 0x23300000

INFO: *0x1080170 = 0x8a090705

INFO: *0x1080174 = 0xc675f605

INFO: *0x1080190 = 0x6070705

INFO: *0x1080194 = 0x5050508

INFO: *0x1080200 = 0x10214

INFO: *0x1080208 = 0x10214

INFO: *0x1080210 = 0x10214

INFO: *0x1080220 = 0x500

INFO: *0x1080224 = 0x4000000

INFO: *0x1080228 = 0x400

INFO: *0x108022c = 0x4000000

INFO: *0x1080230 = 0x400

INFO: *0x1080234 = 0x4000000

INFO: *0x1080238 = 0x400

INFO: *0x108023c = 0x4000000

INFO: *0x1080250 = 0x3114600

INFO: *0x1080270 = 0x80000000

INFO: *0x1080280 = 0xffffffff

INFO: *0x1080284 = 0x77edeebe

INFO: *0x1080288 = 0xff0000

INFO: *0x108028c = 0xffffffff

INFO: *0x1080290 = 0xffff0001

INFO: *0x1080400 = 0x215b558

INFO: *0x1080404 = 0xd88d8000

INFO: *0x1080b20 = 0x8080

INFO: *0x1080b24 = 0x80000000

INFO: *0x1080b28 = 0x80040000

INFO: *0x1080b2c = 0xa181

INFO: *0x1080bf8 = 0x20501

INFO: *0x1080bfc = 0x200

INFO: *0x1080d00 = 0x80060000

INFO: *0x1080d20 = 0xffffffff

INFO: *0x1080d28 = 0xaaaaaaaa

INFO: *0x1080d2c = 0x55555555

INFO: *0x1080d30 = 0xcccccccc

INFO: *0x1080d34 = 0x33333333

INFO: *0x1080d38 = 0x12345678

INFO: *0x1080d3c = 0xabcdef01

INFO: *0x1080d40 = 0xaa55aa55

INFO: *0x1080d44 = 0x55aa55aa

INFO: *0x1080f08 = 0xc

INFO: *0x1080f0c = 0x14000c20

INFO: *0x1080f24 = 0x16001600

INFO: *0x1080f28 = 0x1a001c00

INFO: *0x1080f34 = 0x3000

INFO: *0x1080f48 = 0x1

INFO: *0x1080f4c = 0x11000000

INFO: *0x1080f50 = 0x6000500

INFO: *0x1080f54 = 0xe000f00

INFO: *0x1080f58 = 0xa000a00

INFO: *0x1080f5c = 0xa000a00

INFO: *0x1080f60 = 0x10000000

INFO: *0x1080f70 = 0x700046

NOTICE: 4 GB DDR4, 32-bit, CL=12, ECC off

INFO: Time used by DDR driver 4208 ms

INFO: SoC workaround for Errata A008850 Post-Phase was applied

INFO: RCW BOOT SRC is SD/EMMC

INFO: esdhc_emmc_init

INFO: Card detected successfully

INFO: init done:

NOTICE: BL2: v2.4(release):LSDK-21.08-0-g340b20bcb-dirty

NOTICE: BL2: Built : 17:29:40, Jun 15 2022

NOTICE: BL2D:1

INFO: Configuring TrustZone Controller tzc380

NOTICE: BL2D:2

INFO: BL2: Doing platform setup

INFO: BL2: Loading image id 3

INFO: sd-mmc read done.

 

 

0 Kudos
Reply
1 Reply

2,045 Views
yipingwang
NXP TechSupport
NXP TechSupport

You could use QCVS DDRv tool to assist you to do validation and optimization.

Please refer to the attached user manual.

Please download CW4NET_v2020.06 from the following link and install it on your PC.
https://drive.google.com/file/d/1Kjq1nLYrtIfWAHYrup5Cf-TTEJI9iWiu/view?usp=sharing

Please download armv8 11.5.5 pack form the
following link and open CodeWarrior IDE to install it from Help->Install New
Software->Add->Archive.
https://drive.google.com/file/d/1ZHiYWDOhb27o0oD5Brqjn4_vJzRUCKoY/view?usp=sharing

Please use "read from SPD" method to create a QCVS DDR project, then connect to the target board to do validation.

0 Kudos
Reply