Hi ,
According to "LSDK-KC-REV0.pdf", I have downloaded the pre-built image from nxp.com, and burn it on a LS2088ARDB board. The board can find the SATA disk during booting, but kernel reported some errors as below, then SATA can't work finally.
Did I miss anything?
ata2: SATA link up 3.0 Gbps (SStatus 123 SControl 300)
ata2.00: qc timeout (cmd 0xec)
ata2.00: failed to IDENTIFY (I/O error, err_mask=0x4)
ata2: limiting SATA link speed to 1.5 Gbps
ata2: SATA link up 1.5 Gbps (SStatus 113 SControl 310)
ata2.00: failed to IDENTIFY (I/O error, err_mask=0x100)
ata2: SATA link up 1.5 Gbps (SStatus 113 SControl 310
Software environment:
$ wget http://www.nxp.com/lgfiles/sdk/lsdk1709/firmware_ls2088ardb_uboot_norboot.img
Hardware environment:
Board: LS2088AE Rev1.1-RDB, Board Arch: V1, Board version: F, boot from vBank: 4
Full boot logs:
Please see attachment.
Hello Jin Yanjiang,
It seems that there is hardware compatibility issue between this SATA device and LS2088ARDB Rev F.
Please try whether this device can be recognized under u-boot.
=> scsi info
Device 0: (0:0) Vendor: ATA Prod.: Samsung SSD 850 Rev: EMT0
Type: Hard Disk
Capacity: 238475.1 MB = 232.8 GB (488397168 x 512)
=>
Please try whether other SATA device can work on this target board.
What SATA device did you use now? Is it a SATA 2.0 device?
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
"scsi info" returns nothing. So seems my SATA disk is not compatible with LS2088.
Could you send me a list which contains all compatible SATA devices?
Please contact your local FAE to check whether there is hardware problem on this demo board.
Thanks,
Yiping
Thanks for your reply.
I will have a try and tell you more details.