Raw SerDes Usage on LX2160A

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Raw SerDes Usage on LX2160A

Jump to solution
606 Views
reyesc
Contributor I

Hopefully this isn't too broad of a question (and is in the appropriate place).

I'm currently investigating transferring raw data via SerDes and was hoping someone could point me to some documentation/resources that might help out. Churning through the available docs I see that it's tied pretty tightly to the various protocols (ethernet, pcie, sata, etc) via dpaa2 and I haven't seen much in terms of utilizing the SerDes sans-protocol.

The use case here is pretty basic. At some point in the future the plan is to utilize the 25G and PCIe lanes, however currently the hardware won't be in place and so I'd just like to send some raw data out to verify our connections to those paths coming out of the chip. Basically, a loop-back test.

For what it's worth we're running LSDK 18.04.

Any help/info/guidance would be greatly appreciated. Let me know if more info is needed.

0 Kudos
1 Solution
521 Views
yipingwang
NXP TechSupport
NXP TechSupport

There is a SerDes Validation tool which can be used to send raw data over the interface. You can loop back at near end or far end (if your link partner supports) and check if the bit stream is received correctly.

https://www.nxp.com/docs/en/user-guide/QCVS_SerDes_User_Guide.pdf
https://www.nxp.com/docs/en/application-note/AN5119.pdf

View solution in original post

0 Kudos
2 Replies
569 Views
Irene
NXP Pro Support
NXP Pro Support

There is an application note on our website that might help answer some questions for you. 

https://www.nxp.com/docs/en/application-note/AN13329.pdf

0 Kudos
522 Views
yipingwang
NXP TechSupport
NXP TechSupport

There is a SerDes Validation tool which can be used to send raw data over the interface. You can loop back at near end or far end (if your link partner supports) and check if the bit stream is received correctly.

https://www.nxp.com/docs/en/user-guide/QCVS_SerDes_User_Guide.pdf
https://www.nxp.com/docs/en/application-note/AN5119.pdf

0 Kudos