Question about boot error ("DIMM is not supported by this board") of LS1046ARDB.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about boot error ("DIMM is not supported by this board") of LS1046ARDB.

920 Views
kazuyayamauchi
Contributor II

Hi

We used the following DDR 4 memory instead of DDR 4 memory (MTA18ASF1G72AZ-2G3B1ZG) on LS1046ARDB
  - CT4GDFS8213
  - TS512MLH64V1H

When using these DDR4 memories, we will see the "DIMM is not supported by this board" message.

====  LS1046ARM  ====
1.4.3 DDR memory controller
The chip offers one 32/64-bit DDR controller supporting ECC protected memories. The
32/64-bit DDR4 controller operates at up to 2.1 GT/s. Some key DDR controller features
are as follows:
=====================
If not satisfying the above, I guess that this error message will be output.
However, we think that these DDR4 memories satisfy this spec.

Could you advise us the cause of this error message?


Best Regards,

Labels (1)
0 Kudos
1 Reply

572 Views
ufedor
NXP Employee
NXP Employee

The described issue has to be thoroughly investigated and replicated on the LS1046ARDB locally.

To start the investigation it is required to collect additional information.

Most convenient way to perform aforesaid is by creating a Technical Case referring the following:

How I could create a Service Request? 

0 Kudos