QorIQ SENSEVDD and SENSEGND pins electrical characteristics

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QorIQ SENSEVDD and SENSEGND pins electrical characteristics

2,254 Views
fdm
Contributor IV

Hi,

What is the order of magnitude of the SENSEVDD/SENSEGND pins output impedance and what current levels they can safely source/sink (first and foremost, for QorIQ T1040 and/or LS1021A)?

BR,
   Denis

Labels (1)
Tags (3)
0 Kudos
Reply
4 Replies

2,050 Views
ufedor
NXP Employee
NXP Employee

Please note that the SENSE signals are just connected to the corresponding VDD and GND on-chip networks somewhere in the middle of the cores' "cluster".

0 Kudos
Reply

2,050 Views
fdm
Contributor IV

The question is just about electrical characteristics of this connection.

Could we assume that the impedance value is on the order of hundreds of milliohms (or a few ohms in the worst case)?

0 Kudos
Reply

2,049 Views
ufedor
NXP Employee
NXP Employee

Impedance of what?

Please understand that these signals can be considered as ordinary VDD and GND pins.

0 Kudos
Reply

2,050 Views
fdm
Contributor IV

I'm trying to evaluate the influence of an external sensing circuit input impedance on the measurement accuracy.

Given that these signals in essence are power pins, I believe that my estimation is close to reality.

0 Kudos
Reply