I'm looking to download the source release for the QorIQ SDK for my LS1043A processor, but I don't see a source release on the download page (https://nxp.flexnetoperations.com/control/frse/download?element=7726177). All I see is the cache and the image.
I know v2.0 is just being released, will a source download be provided soon? Or should one be displayed now?
Please re-visit the page. There are 18 files, the source ISO image is at the very bottom. If you don't see it, clear your
browser cache or use another browser/machine
Have a great day,
Platon
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------