I want to use the QorIQ SDK 2.0 in Ubuntu 18.04 for ls1021a, but its throwing error while setting up. SO is their any possibility to use Ubuntu 18 and 20.
Regards
Winston
---------------------------------
C 00326829 Community: QorIQ Processing Platforms
Subject
[Community] QorIQ SDK 2.0 though error in Ubuntu 16, 18 and 20
Description
I want to use the QorIQ SDK 2.0 in Ubuntu 18.04 for ls1021a, but its throwing error while setting up. SO is their any possibility to use Ubuntu 18 and 20.
============
Use Ubuntu 14 for SDK building. Do not use Ubuntu 16 or Ubuntu 18.
The following command sequence was used under Ubuntu 14:
Message: /bin/sh -> dash
Answer after password – No
Message:
Removing 'diversion of /bin/sh to /bin/sh.distrib by dash'
Adding 'diversion of /bin/sh to /bin/sh.distrib by bash'
Removing 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by dash'
Adding 'diversion of /usr/share/man/man1/sh.1.gz to /usr/share/man/man1/sh.distrib.1.gz by bash'
Message: /bin/sh -> bash
Usually Linux recommends also run the following command: sudo usr/sbin/visudo
Linux kernel code is available using the following path:
/QorIQ-SDK-V2.0-20160527-yocto/build_ls1043ardb/tmp/work/ls1043ardb-fsl-linux/linux-qoriq/4.1-r0/git
Source code of u-boot is available using the following path:
/QorIQ-SDK-V2.0-20160527-yocto/build_ls1046ardb/tmp/work/ls1046ardb-fsl-linux/u-boot-qoriq/2016.09+fslgit-r0/git
Note: NXP offers also Yocto SDK 2.7:
https://source.codeaurora.org/external/qoriq/qoriq-components/yocto-sdk/about/
This SDK can be used under Ubuntu 16, 18 and 20