QCVS validation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,956件の閲覧回数
muaxi8
Contributor V

Platform: LX2160A customized board card。and my ddr4 is discrete type.

I did the validation with QCVS, then what should I do to use the calibrated value.

muaxi8_0-1626241692981.png

 

0 件の賞賛
返信
1 解決策
1,925件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

This should be the code for the slave core, entering into sleep mode. Please attach to the master core to check the problem code.

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
1,947件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

Please refer to section "1.1.1.2 Configure DDR controller" in the attached QCVS DDRv user guide.

After creating a QCVS DDR project for Discreate DRAM with the default parameters, please fill "Properties" panel according to your DDR Datasheet.

0 件の賞賛
返信
1,944件の閲覧回数
muaxi8
Contributor V

hi yipingwnag:

how to use codewarrior to debug uboot ? my pbl It's already ok, but my uboot can  not start up.

0 件の賞賛
返信
1,940件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
1,933件の閲覧回数
muaxi8
Contributor V

hello.

when i debugging uboot with codeworrior, my uboot  is wrong here: cbz x0, slave_cpu.

What does the mean of "slave_cpu",  What cause the wrong here?

thanks.

muaxi8_0-1626351894105.png

 

0 件の賞賛
返信
1,912件の閲覧回数
muaxi8
Contributor V

 

 

 

 

0 件の賞賛
返信
1,926件の閲覧回数
yipingwang
NXP TechSupport
NXP TechSupport

This should be the code for the slave core, entering into sleep mode. Please attach to the master core to check the problem code.

0 件の賞賛
返信