Purpose of sw_svr in LS1043ARDB-PD reference board

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Purpose of sw_svr in LS1043ARDB-PD reference board

Jump to solution
526 Views
Abhilash_PV
Contributor I

sw_svr signal in the CPLD of LS1043ARDB-PD reference board is assigned to ifc_a[16] and ifc_a[17] of the processor. What is the action from LS1043A based on it? Which source file specifies the code defining this action?

0 Kudos
1 Solution
520 Views
ufedor
NXP Employee
NXP Employee

Functionality of the cfg_svr[0:1] was defeatured.

Current requirement in QorIQ LS1043A, LS1023A Data Sheet is:

Pin must NOT be pulled down during power-on reset.

View solution in original post

0 Kudos
2 Replies
521 Views
ufedor
NXP Employee
NXP Employee

Functionality of the cfg_svr[0:1] was defeatured.

Current requirement in QorIQ LS1043A, LS1023A Data Sheet is:

Pin must NOT be pulled down during power-on reset.

0 Kudos
517 Views
Abhilash_PV
Contributor I

Thank you for the update.

0 Kudos