Hi, I’m working on LS1021A-Twr hardware using QorIQ SDK-V1.7, according to Ls1021aatwr document SDboot is supported, I’m facing few issues w.r.t SDBOOT.
Following is my set-up description:
a) Hardware: LS1021A-TWR
b) Kernel-3.12.19, u-boot:2014.07
c) Booting u-boot,kernel and Rootfs are from the SD-CARD.
d) Rootfs uses Systemd
Problem Description:
1) With same kernel,rootfs booting from SDCARD, Audio card is not getting detected in case of u-boot compiled and booted from SDCARD, and is working perfectly with u-boot compiled and booted from NOR:
Sound Log Snippet when u-boot from NOR, Kernel & Rootfs SDCARD:
sgtl5000 1-000a: sgtl5000 revision 0x11
mmc0: new high speed SDHC card at address aaaa
sgtl5000 1-000a: Failed to get supply 'VDDD': -19
mmcblk0: mmc0:aaaa SU08G 7.40 GiB
1-000a: 1200 mV normal
sgtl5000 1-000a: Using internal LDO instead of VDDD
mmcblk0: p1 p2
vf610-sgtl5000 sound.9: sgtl5000 <-> 2b50000.sai mapping ok
oprofile: using timer interrupt.
TCP: cubic registered
Initializing XFRM netlink socket
NET: Registered protocol family 17
NET: Registered protocol family 15
can: controller area network core (rev 20120528 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20120528)
Key type dns_resolver registered
regulator-dummy: disabling
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
ALSA device list:
#0: FSL-VF610-TWR-BOARD
Sound Log Snippet when u-boot From SD, kernel & ROOTFS SDCARD:
sgtl5000: probe of 1-000a failed with error -110
vf610-sgtl5000 sound.9: ASoC: CODEC (null) not registered
vf610-sgtl5000 sound.9: TWR-AUDIO-SGTL board required :-517
platform sound.9: Driver vf610-sgtl5000 requests probe deferral
oprofile: using timer interrupt.
TCP: cubic registered
Initializing XFRM netlink socket
NET: Registered protocol family 17
NET: Registered protocol family 15
can: controller area network core (rev 20120528 abi 9)
NET: Registered protocol family 29
can: raw protocol (rev 20120528)
Key type dns_resolver registered
regulator-dummy: disabling
vf610-sgtl5000 sound.9: ASoC: CODEC (null) not registered
vf610-sgtl5000 sound.9: TWR-AUDIO-SGTL board required :-517
platform sound.9: Driver vf610-sgtl5000 requests probe deferral
drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
ALSA device list:
No soundcards found.
2) Compared the rcw_1000.rcw and rcw_1000_sdboot.rcw important difference seemed to be in LVDD_SEL modified it accordingly but there wasn’t any change.
3) Understood that U-boot-spl-pbl.bin which is used for SDBOOT is a combination of rcw+u-boot, can you let me know the process to independently flashing the rcw_1000_sdboot.bin with u-boot compiled for SDcard.
4) Also observed recursive crashes w.r.t CPU idle, when I left the board booted from SDCARD idle for 15-20mins when CPU trying to enter idle mode it was crashing,Please find below the crash log:
root@ls1021atwr:~# dmesg | grep -i sgtl
sgtl5000: probe of 1-000a failed with error -110
vf610-sgtl5000 sound.9: ASoC: CODEC (null) not registered
vf610-sgtl5000 sound.9: TWR-AUDIO-SGTL board required :-517
platform sound.9: Driver vf610-sgtl5000 requests probe deferral
vf610-sgtl5000 sound.9: ASoC: CODEC (null) not registered
vf610-sgtl5000 sound.9: TWR-AUDIO-SGTL board required :-517
platform sound.9: Driver vf610-sgtl5000 requests probe deferral
vf610-sgtl5000 sound.9: ASoC: CODEC (null) not registered
vf610-sgtl5000 sound.9: TWR-AUDIO-SGTL board required :-517
platform sound.9: Driver vf610-sgtl5000 requests probe deferral
root@ls1021atwr:~# INFO: rcu_sched self-detected stall on CPU { 0} (t=2100 jiffies g=0 c=4294967295 q=11)
CPU: 0 PID: 0 Comm: swapper/0 Not tainted 3.12.19-rt30+ #2
[<80010699>] (unwind_backtrace+0x1/0x8c) from [<8000e3ff>] (show_stack+0xb/0xc)
[<8000e3ff>] (show_stack+0xb/0xc) from [<80301fdf>] (dump_stack+0x4b/0x60)
[<80301fdf>] (dump_stack+0x4b/0x60) from [<80052217>] (rcu_check_callbacks+0x121/0x3f2)
[<80052217>] (rcu_check_callbacks+0x121/0x3f2) from [<8001fa1b>] (update_process_times+0x2b/0x44)
[<8001fa1b>] (update_process_times+0x2b/0x44) from [<8004438b>] (tick_periodic+0x6b/0x88)
[<8004438b>] (tick_periodic+0x6b/0x88) from [<800444a9>] (tick_handle_periodic+0x19/0x64)
[<800444a9>] (tick_handle_periodic+0x19/0x64) from [<80258a17>] (arch_timer_handler_phys+0x1f/0x26)
[<80258a17>] (arch_timer_handler_phys+0x1f/0x26) from [<8003d48f>] (handle_percpu_devid_irq+0x3f/0x54)
[<8003d48f>] (handle_percpu_devid_irq+0x3f/0x54) from [<8003b1e3>] (generic_handle_irq+0x13/0x1c)
[<8003b1e3>] (generic_handle_irq+0x13/0x1c) from [<8000c8fd>] (handle_IRQ+0x3d/0x60)
[<8000c8fd>] (handle_IRQ+0x3d/0x60) from [<800083d3>] (gic_handle_irq+0x2b/0x44)
[<800083d3>] (gic_handle_irq+0x2b/0x44) from [<80304d5b>] (__irq_svc+0x3b/0x5c)
Exception stack(0x804d1eb0 to 0x804d1ef8)
1ea0: 00000001 00200000 00000100 00000000
1ec0: 804d0018 00000000 00000082 80511100 80003010 410fc075 0000000a 00000000
1ee0: 00000000 804d1ef8 8001b29f 8001b2de 400d0133 ffffffff
[<80304d5b>] (__irq_svc+0x3b/0x5c) from [<8001b2de>] (__do_softirq+0x52/0x120)
[<8001b2de>] (__do_softirq+0x52/0x120) from [<8001b411>] (do_softirq+0x2d/0x38)
[<8001b411>] (do_softirq+0x2d/0x38) from [<8001b93d>] (irq_exit+0x4f/0x8e)
[<8001b93d>] (irq_exit+0x4f/0x8e) from [<8000c901>] (handle_IRQ+0x41/0x60)
[<8000c901>] (handle_IRQ+0x41/0x60) from [<800083d3>] (gic_handle_irq+0x2b/0x44)
[<800083d3>] (gic_handle_irq+0x2b/0x44) from [<80304d5b>] (__irq_svc+0x3b/0x5c)
Exception stack(0x804d1f70 to 0x804d1fb8)
1f60: ffffffed 00000000 00884000 00000000
1f80: 804d0000 804d0000 804c1510 80d4dcc0 80003010 410fc075 00000000 00000000
1fa0: 00000008 804d1fb8 8000cae5 8000cae6 600d0033 ffffffff
[<80304d5b>] (__irq_svc+0x3b/0x5c) from [<8000cae6>] (arch_cpu_idle+0x1a/0x20)
[<8000cae6>] (arch_cpu_idle+0x1a/0x20) from [<8003b17d>] (cpu_startup_entry+0x7d/0xc4)
[<8003b17d>] (cpu_startup_entry+0x7d/0xc4) from [<804a1811>] (start_kernel+0x219/0x26c)
INFO: rcu_sched self-detected stall on CPU { 0} (t=8403 jiffies g=0 c=4294967295 q=19)
CPU: 0 PID: 0 Comm: swapper/0 Not tainted 3.12.19-rt30+ #2
[<80010699>] (unwind_backtrace+0x1/0x8c) from [<8000e3ff>] (show_stack+0xb/0xc)
[<8000e3ff>] (show_stack+0xb/0xc) from [<80301fdf>] (dump_stack+0x4b/0x60)
[<80301fdf>] (dump_stack+0x4b/0x60) from [<80052217>] (rcu_check_callbacks+0x121/0x3f2)
[<80052217>] (rcu_check_callbacks+0x121/0x3f2) from [<8001fa1b>] (update_process_times+0x2b/0x44)
[<8001fa1b>] (update_process_times+0x2b/0x44) from [<8004438b>] (tick_periodic+0x6b/0x88)
[<8004438b>] (tick_periodic+0x6b/0x88) from [<800444a9>] (tick_handle_periodic+0x19/0x64)
[<800444a9>] (tick_handle_periodic+0x19/0x64) from [<80258a17>] (arch_timer_handler_phys+0x1f/0x26)
[<80258a17>] (arch_timer_handler_phys+0x1f/0x26) from [<8003d48f>] (handle_percpu_devid_irq+0x3f/0x54)
[<8003d48f>] (handle_percpu_devid_irq+0x3f/0x54) from [<8003b1e3>] (generic_handle_irq+0x13/0x1c)
[<8003b1e3>] (generic_handle_irq+0x13/0x1c) from [<8000c8fd>] (handle_IRQ+0x3d/0x60)
[<8000c8fd>] (handle_IRQ+0x3d/0x60) from [<800083d3>] (gic_handle_irq+0x2b/0x44)
[<800083d3>] (gic_handle_irq+0x2b/0x44) from [<80304d5b>] (__irq_svc+0x3b/0x5c)
Exception stack(0x804d1eb0 to 0x804d1ef8)
1ea0: 00000001 00200000 00000100 00000000
1ec0: 804d0018 00000000 00000082 80511100 80003010 410fc075 0000000a 00000000
1ee0: 00000000 804d1ef8 8001b29f 8001b2de 400d0133 ffffffff
[<80304d5b>] (__irq_svc+0x3b/0x5c) from [<8001b2de>] (__do_softirq+0x52/0x120)
[<8001b2de>] (__do_softirq+0x52/0x120) from [<8001b411>] (do_softirq+0x2d/0x38)
[<8001b411>] (do_softirq+0x2d/0x38) from [<8001b93d>] (irq_exit+0x4f/0x8e)
[<8001b93d>] (irq_exit+0x4f/0x8e) from [<8000c901>] (handle_IRQ+0x41/0x60)
[<8000c901>] (handle_IRQ+0x41/0x60) from [<800083d3>] (gic_handle_irq+0x2b/0x44)
[<800083d3>] (gic_handle_irq+0x2b/0x44) from [<80304d5b>] (__irq_svc+0x3b/0x5c)
Exception stack(0x804d1f70 to 0x804d1fb8)
1f60: ffffffed 00000000 00884000 00000000
1f80: 804d0000 804d0000 804c1510 80d4dcc0 80003010 410fc075 00000000 00000000
1fa0: 00000008 804d1fb8 8000cae5 8000cae6 600d0033 ffffffff
[<80304d5b>] (__irq_svc+0x3b/0x5c) from [<8000cae6>] (arch_cpu_idle+0x1a/0x20)
[<8000cae6>] (arch_cpu_idle+0x1a/0x20) from [<8003b17d>] (cpu_startup_entry+0x7d/0xc4)
[<8003b17d>] (cpu_startup_entry+0x7d/0xc4) from [<804a1811>] (start_kernel+0x219/0x26c)
INFO: rcu_sched self-detected stall on CPU { 0} (t=14706 jiffies g=0 c=4294967295 q=31)
CPU: 0 PID: 0 Comm: swapper/0 Not tainted 3.12.19-rt30+ #2
[<80010699>] (unwind_backtrace+0x1/0x8c) from [<8000e3ff>] (show_stack+0xb/0xc)
[<8000e3ff>] (show_stack+0xb/0xc) from [<80301fdf>] (dump_stack+0x4b/0x60)
[<80301fdf>] (dump_stack+0x4b/0x60) from [<80052217>] (rcu_check_callbacks+0x121/0x3f2)
[<80052217>] (rcu_check_callbacks+0x121/0x3f2) from [<8001fa1b>] (update_process_times+0x2b/0x44)
[<8001fa1b>] (update_process_times+0x2b/0x44) from [<8004438b>] (tick_periodic+0x6b/0x88)
[<8004438b>] (tick_periodic+0x6b/0x88) from [<800444a9>] (tick_handle_periodic+0x19/0x64)
[<800444a9>] (tick_handle_periodic+0x19/0x64) from [<80258a17>] (arch_timer_handler_phys+0x1f/0x26)
[<80258a17>] (arch_timer_handler_phys+0x1f/0x26) from [<8003d48f>] (handle_percpu_devid_irq+0x3f/0x54)
[<8003d48f>] (handle_percpu_devid_irq+0x3f/0x54) from [<8003b1e3>] (generic_handle_irq+0x13/0x1c)
[<8003b1e3>] (generic_handle_irq+0x13/0x1c) from [<8000c8fd>] (handle_IRQ+0x3d/0x60)
[<8000c8fd>] (handle_IRQ+0x3d/0x60) from [<800083d3>] (gic_handle_irq+0x2b/0x44)
[<800083d3>] (gic_handle_irq+0x2b/0x44) from [<80304d5b>] (__irq_svc+0x3b/0x5c)
Exception stack(0x804d1eb0 to 0x804d1ef8)
1ea0: 00000001 00200000 00000100 00000000
1ec0: 804d0018 00000000 00000082 80511100 80003010 410fc075 0000000a 00000000
1ee0: 00000000 804d1ef8 8001b29f 8001b2de 400d0133 ffffffff
[<80304d5b>] (__irq_svc+0x3b/0x5c) from [<8001b2de>] (__do_softirq+0x52/0x120)
[<8001b2de>] (__do_softirq+0x52/0x120) from [<8001b411>] (do_softirq+0x2d/0x38)
[<8001b411>] (do_softirq+0x2d/0x38) from [<8001b93d>] (irq_exit+0x4f/0x8e)
[<8001b93d>] (irq_exit+0x4f/0x8e) from [<8000c901>] (handle_IRQ+0x41/0x60)
[<8000c901>] (handle_IRQ+0x41/0x60) from [<800083d3>] (gic_handle_irq+0x2b/0x44)
[<800083d3>] (gic_handle_irq+0x2b/0x44) from [<80304d5b>] (__irq_svc+0x3b/0x5c)
Exception stack(0x804d1f70 to 0x804d1fb8)
1f60: ffffffed 00000000 00884000 00000000
1f80: 804d0000 804d0000 804c1510 80d4dcc0 80003010 410fc075 00000000 00000000
1fa0: 00000008 804d1fb8 8000cae5 8000cae6 600d0033 ffffffff
[<80304d5b>] (__irq_svc+0x3b/0x5c) from [<8000cae6>] (arch_cpu_idle+0x1a/0x20)
[<8000cae6>] (arch_cpu_idle+0x1a/0x20) from [<8003b17d>] (cpu_startup_entry+0x7d/0xc4)
[<8003b17d>] (cpu_startup_entry+0x7d/0xc4) from [<804a1811>] (start_kernel+0x219/0x26c)
Hi Adrian,
I see that most of the examples are for Power-PC architecture, are the instructions similar for the LS1021 also? Also wanted to check whether complete booting via SD is supported?
Regards,
Arun.
Hello khandavalli arun,
Sorry for the late reply.
Please check whether the above information would be helpful for you.
Thanks,
Yiping
Hi Yiping,
Sorry was struck up with something else, I have already tried both the solutions which you have given but there was no effect.
1) Audio Via SDCARD:
I have also compared the rcw_1000.rcw and rcw_1000_sd.rcw made changes accordingly and verifed, but still audio card wassnt getting detected.But I have seen that I2C2 is the adapter for both the sgtl-5000codec & SDHC_WP and SDHC_CD_N SD. Is the configuration not set properly when booted via SD? I also need to dig more further in the u-boot.
4) RCU STALL:
ls1021atwr login: root
root@ls1021atwr:~# zcat /proc/con
config.gz consoles
root@ls1021atwr:~# zcat /proc/con
config.gz consoles
root@ls1021atwr:~# zcat /proc/config.gz | grep -i idle
# CONFIG_NO_HZ_IDLE is not set
CONFIG_GENERIC_SMP_IDLE_THREAD=y
CONFIG_GENERIC_IDLE_POLL_SETUP=y
# CPU Idle
CONFIG_CPU_IDLE=y
# CONFIG_CPU_IDLE_MULTIPLE_DRIVERS is not set
CONFIG_CPU_IDLE_GOV_LADDER=y
CONFIG_CPU_IDLE_GOV_MENU=y
# ARM CPU Idle Drivers
# CONFIG_ARCH_NEEDS_CPU_IDLE_COUPLED is not set
root@ls1021atwr:~#
root@ls1021atwr:~#
root@ls1021atwr:~#
root@ls1021atwr:~#
root@ls1021atwr:~#
root@ls1021atwr:~#
root@ls1021atwr:~#
root@ls1021atwr:~#
root@ls1021atwr:~#
root@ls1021atwr:~#
root@ls1021atwr:~#
root@ls1021atwr:~# INFO: rcu_sched self-detected stall on CPU { 0} (t=2100 jiffies g=8 c=7 q=9)
CPU: 0 PID: 0 Comm: swapper/0 Not tainted 3.12.19-rt30+ #3
[<80010699>] (unwind_backtrace+0x1/0x8c) from [<8000e3ff>] (show_stack+0xb/0xc)
[<8000e3ff>] (show_stack+0xb/0xc) from [<80300ccf>] (dump_stack+0x4b/0x60)
[<80300ccf>] (dump_stack+0x4b/0x60) from [<80050fcb>] (rcu_check_callbacks+0x121/0x3f2)
[<80050fcb>] (rcu_check_callbacks+0x121/0x3f2) from [<8001f7e3>] (update_process_times+0x2b/0x44)
[<8001f7e3>] (update_process_times+0x2b/0x44) from [<800438d3>] (tick_periodic+0x6b/0x88)
[<800438d3>] (tick_periodic+0x6b/0x88) from [<800439f1>] (tick_handle_periodic+0x19/0x64)
[<800439f1>] (tick_handle_periodic+0x19/0x64) from [<80257703>] (arch_timer_handler_phys+0x1f/0x26)
[<80257703>] (arch_timer_handler_phys+0x1f/0x26) from [<8003c9d7>] (handle_percpu_devid_irq+0x3f/0x54)
[<8003c9d7>] (handle_percpu_devid_irq+0x3f/0x54) from [<8003a72b>] (generic_handle_irq+0x13/0x1c)
[<8003a72b>] (generic_handle_irq+0x13/0x1c) from [<8000c8fd>] (handle_IRQ+0x3d/0x60)
[<8000c8fd>] (handle_IRQ+0x3d/0x60) from [<800083d3>] (gic_handle_irq+0x2b/0x44)
[<800083d3>] (gic_handle_irq+0x2b/0x44) from [<80303a5b>] (__irq_svc+0x3b/0x5c)
Exception stack(0x804d3eb0 to 0x804d3ef8)
3ea0: 00000001 00200000 00000100 00000000
3ec0: 804d2018 00000000 00000082 80513100 80003010 410fc075 0000000a 00000000
3ee0: 00000000 804d3ef8 8001b263 8001b2a2 400e0133 ffffffff
[<80303a5b>] (__irq_svc+0x3b/0x5c) from [<8001b2a2>] (__do_softirq+0x52/0x120)
[<8001b2a2>] (__do_softirq+0x52/0x120) from [<8001b3d5>] (do_softirq+0x2d/0x38)
[<8001b3d5>] (do_softirq+0x2d/0x38) from [<8001b901>] (irq_exit+0x4f/0x6e)
[<8001b901>] (irq_exit+0x4f/0x6e) from [<8000c901>] (handle_IRQ+0x41/0x60)
[<8000c901>] (handle_IRQ+0x41/0x60) from [<800083d3>] (gic_handle_irq+0x2b/0x44)
[<800083d3>] (gic_handle_irq+0x2b/0x44) from [<80303a5b>] (__irq_svc+0x3b/0x5c)
Exception stack(0x804d3f70 to 0x804d3fb8)
3f60: ffffffed 00000000 00883000 00000000
3f80: 804d2000 804d2000 804c44d0 80d4fd00 80003010 410fc075 00000000 00000000
3fa0: 804d2044 804d3fb8 8000cae5 8000cae6 600e0033 ffffffff
[<80303a5b>] (__irq_svc+0x3b/0x5c) from [<8000cae6>] (arch_cpu_idle+0x1a/0x20)
[<8000cae6>] (arch_cpu_idle+0x1a/0x20) from [<8003a6c9>] (cpu_startup_entry+0x79/0xbc)
[<8003a6c9>] (cpu_startup_entry+0x79/0xbc) from [<804a4811>] (start_kernel+0x219/0x26c)
INFO: rcu_sched self-detected stall on CPU { 0} (t=8403 jiffies g=
Hi Yiping,
Regarding RCU Stall detecttion, I have further enabled the debugging configs, following is the debug trace for the same:
root@ls1021atwr:~# BUG: soft lockup - CPU#0 stuck for 23s! [swapper/0:0]
Modules linked in:
CPU: 0 PID: 0 Comm: swapper/0 Not tainted 3.12.19-rt30+ #5
task: 804d3260 ti: 804c8000 task.ti: 804c8000
PC is at __do_softirq+0x52/0x120
LR is at __do_softirq+0x13/0x120
pc : [<8001af8a>] lr : [<8001af4b>] psr: 400f0133
sp : 804c9ef8 ip : 00000000 fp : 00000000
r10: 0000000a r9 : 410fc075 r8 : 80003010
r7 : 8050c040 r6 : 00000082 r5 : 00000000 r4 : 804c8018
r3 : 00000000 r2 : 00000100 r1 : 00200000 r0 : 00000001
Flags: nZcv IRQs on FIQs on Mode SVC_32 ISA Thumb Segment kernel
Control: 70c53c7d Table: bf1bf080 DAC: fffffffd
CPU: 0 PID: 0 Comm: swapper/0 Not tainted 3.12.19-rt30+ #5
[<80010681>] (unwind_backtrace+0x1/0x8c) from [<8000e3f7>] (show_stack+0xb/0xc)
[<8000e3f7>] (show_stack+0xb/0xc) from [<802f7c37>] (dump_stack+0x4b/0x60)
[<802f7c37>] (dump_stack+0x4b/0x60) from [<8004cd65>] (watchdog_timer_fn+0xad/0xe8)
[<8004cd65>] (watchdog_timer_fn+0xad/0xe8) from [<8002b093>] (hrtimer_run_queues+0xcf/0x144)
[<8002b093>] (hrtimer_run_queues+0xcf/0x144) from [<8001f243>] (run_local_timers+0xf/0x34)
[<8001f243>] (run_local_timers+0xf/0x34) from [<8001f28b>] (update_process_times+0x23/0x44)
[<8001f28b>] (update_process_times+0x23/0x44) from [<80041a41>] (tick_periodic+0x5f/0x7e)
[<80041a41>] (tick_periodic+0x5f/0x7e) from [<80041b11>] (tick_handle_periodic+0x19/0x64)
[<80041b11>] (tick_handle_periodic+0x19/0x64) from [<80250197>] (arch_timer_handler_phys+0x1f/0x26)
[<80250197>] (arch_timer_handler_phys+0x1f/0x26) from [<8003b0b7>] (handle_percpu_devid_irq+0x3f/0x54)
[<8003b0b7>] (handle_percpu_devid_irq+0x3f/0x54) from [<80038e9f>] (generic_handle_irq+0x13/0x1c)
[<80038e9f>] (generic_handle_irq+0x13/0x1c) from [<8000c8fd>] (handle_IRQ+0x3d/0x60)
[<8000c8fd>] (handle_IRQ+0x3d/0x60) from [<800083d3>] (gic_handle_irq+0x2b/0x44)
[<800083d3>] (gic_handle_irq+0x2b/0x44) from [<802fa61b>] (__irq_svc+0x3b/0x5c)
Exception stack(0x804c9eb0 to 0x804c9ef8)
9ea0: 00000001 00200000 00000100 00000000
9ec0: 804c8018 00000000 00000082 8050c040 80003010 410fc075 0000000a 00000000
9ee0: 00000000 804c9ef8 8001af4b 8001af8a 400f0133 ffffffff
[<802fa61b>] (__irq_svc+0x3b/0x5c) from [<8001af8a>] (__do_softirq+0x52/0x120)
[<8001af8a>] (__do_softirq+0x52/0x120) from [<8001b0bd>] (do_softirq+0x2d/0x38)
[<8001b0bd>] (do_softirq+0x2d/0x38) from [<8001b5e1>] (irq_exit+0x4f/0x6e)
[<8001b5e1>] (irq_exit+0x4f/0x6e) from [<8000c901>] (handle_IRQ+0x41/0x60)
[<8000c901>] (handle_IRQ+0x41/0x60) from [<800083d3>] (gic_handle_irq+0x2b/0x44)
[<800083d3>] (gic_handle_irq+0x2b/0x44) from [<802fa61b>] (__irq_svc+0x3b/0x5c)
Exception stack(0x804c9f70 to 0x804c9fb8)
9f60: ffffffed 00000000 0088d000 00000000
9f80: 804c8000 804c8000 804b8918 80d4fcc0 80003010 410fc075 00000000 00000000
9fa0: 804c8044 804c9fb8 8000cad5 8000cad6 600f0033 ffffffff
[<802fa61b>] (__irq_svc+0x3b/0x5c) from [<8000cad6>] (arch_cpu_idle+0x1a/0x20)
[<8000cad6>] (arch_cpu_idle+0x1a/0x20) from [<80038e3d>] (cpu_startup_entry+0x6d/0xb0)
[<80038e3d>] (cpu_startup_entry+0x6d/0xb0) from [<8049e811>] (start_kernel+0x219/0x26c)
mmc0: Timeout waiting for hardware interrupt.
INFO: rcu_sched self-detected stall on CPU
0: (1 GPs behind) idle=f3f/2/0 softirq=0/0
(t=2100 jiffies g=20 c=19 q=28)
Hello khandavalli arun,
1)2) I also found RCW[DVDD_VSEL] is different, probably this is the root cause.
3. In SDK 1.7, the file U-boot-spl-pbl.bin is built directly from u-boot source code, you could modify the file board/freescale/ls1021atwr/ls102xa_rcw_sd.cfg.
If you use SDK build environment, you could use the following steps.
$ bitbake u-boot -c cleansstate
Modify the "UBOOT_CONFIG" as "sdcard" in meta-fsl-arm/conf/machine/ls1021atwr.conf.
$ bitbake u-boot -c patch
Go to the folder build_ls1021atwr_release/tmp/work/ls1021atwr-fsl-linux-gnueabi/u-boot-ls1/2013.10-r0/git and modify the file board/freescale/ls1021atwr/ls102xa_rcw_sd.cfg.
$ bitbake u-boot
After rebuild u-boot, you will get image u-boot-with-spl-pbl.bin in u-boot source folder.
4. Please check whether it would be helpful to use "nohz=off" Kernel boot parameter to disable dyntick-idle mode.
This boot parameter "nohz=" that can be used to disable dyntick-idle mode in CONFIG_NO_HZ_IDLE=y kernel by specifying "nohz=off". By the default, the system boot with "nohz=on", enabling dyntick-idle mode.
An idle CPU that is not receiving scheduling-clock interrupts is said to be "dyntick-idle". The CONFIG_NO_HZ_IDLE=y Kconfig option causes the kernel to avoid sending scheduling-clock interrupts to idle CPUs, which is critically important both to battery-powered devices and to highly virtualized mainframes.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------